EAGLE User Support (English) Idea to improve exploration of the EAGLE libraries
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
  • State Suggested Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 179 subscribers
  • Views 519 views
  • Users 0 members are here
Related

Idea to improve exploration of the EAGLE libraries

Former Member
Former Member over 12 years ago

Hello,

 

Incorporating a second vertical bar at each library facilitates the exploration, Because scans independently each library, rather than explore the full vertical bar

 

It is a good idea +1 or -1?

 

Screenshothttp://jaimeza.org/Temp/Request/Request_eagle_cadsoft_multiverticalbar.gif

 

 

Note The vertical bar (main) on the right explores the whole of libraries

 

+1, please vote

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 12 years ago

    I think it would be breaking many design rules. The left expansion triangle would expand but not expose everything, which is not what people are accustomed to on any OS. I could see it having some value if one wanted to (say) compare the v-reg library with the varistor library on the same screen simultaneously as shown in the screenshot, but currently I can't think of any use-case for that. Plus, it would break down with smaller screen laptops, where people may resize that window to be a fraction of the size of the screenshot currently.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 12 years ago

    I think it would be breaking many design rules. The left expansion triangle would expand but not expose everything, which is not what people are accustomed to on any OS. I could see it having some value if one wanted to (say) compare the v-reg library with the varistor library on the same screen simultaneously as shown in the screenshot, but currently I can't think of any use-case for that. Plus, it would break down with smaller screen laptops, where people may resize that window to be a fraction of the size of the screenshot currently.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 12 years ago in reply to shabaz

    Sorry for my bad English image

     

    >> The left expansion triangle would expand but not expose everything,

    The idea isnot to expand the entire list, if not part of it, to facilitate vertical scanning, In the animation I made can be seen better

     

    When the library list is extensive, it loses his focus, difficult to exploration, my idea has a better view of the library "tree"

     

    PD: New updated image (gif of 26 images) ^

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer