EAGLE User Support (English) Newbie question : "Supply pin VCC overwritten with more than one signal"
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
  • State Not Answered
  • Replies 2 replies
  • Subscribers 181 subscribers
  • Views 680 views
  • Users 0 members are here
Related

Newbie question : "Supply pin VCC overwritten with more than one signal"

BigJon
BigJon over 13 years ago

Hi,

 

I have a board with some components that all have a "VCC" pin. However some componets are 3.3v and some 5v. When I connect the VCC pins to the 5v or 3.3v supplies I get asked if I want to rename the resultant net. I answered to rename them to "3.3v" and "5v" which made sense and are the names of my power supply nets.

 

However when I run the rules checker I get an error. IIUIC it thinks the "VCC" net has both 5v and 3.3v connections ?

 

How do I get round this and have mixed 3.3v and 5v VCC pins ?

 

Thanks.

 

Jon.

 

 

5v GPS :

image

3.3v Xbee :

image

 

Errors :

image

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 13 years ago

    try putting the 5V in parenthases.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 13 years ago

    try putting the 5V in parenthases.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dukepro
    0 dukepro over 13 years ago in reply to Former Member

    On 01/23/2013 04:55 AM, Grant Pay wrote:

    try putting the 5V in parenthases.

     

     

    I could not find in the manual any mention of the use of parentheses on

    supply signals.  Can you explain what this does, or perhaps refer me to

    a section in the manual?

     

    Thanks,

        - Chuck