Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Small Ring Pad - not small enough
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 401 views
  • Users 0 members are here
  • pad
  • pcb_traces
  • drc
Related

Small Ring Pad - not small enough

e14 Contributor
e14 Contributor over 13 years ago

Hi,

I'm working on a project with 6.4 that was started in 6.3 - hopefully that won't make a difference.

 

What I want to do is create a pad with a very small ring.

 

In addition, I am trying to do this as part of a library device, so it should be easy.

 

When I draw the package (library editor), I can show Pads any way I like - eg. square pad with drill diam. larger than Pad edge, resulting in a 'Pad' with only the corners attached to a hole.

This is an exaggeration of what I really want, but makes the point.

 

When I use the device on a .brd, the properties of the Pad are overridden.

 

I've played with Restring values in DRC. I can grow the OD, but can't get it down to the size shown in the Library package.

 

Is there something obvious I'm missing?

 

An alternative approach would be a plated through hole with no ring at all (I'm not sure that's possible).

 

cheers,

 

ian

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    On 08.02.2013 12:45, ian . wrote:

    Hi,

    I'm working on a project with 6.3 that was started in 6.2 - hopefully that won't make a difference.

     

    What I want to do is create a pad with a very small ring.

     

    In addition, I am trying to do this as part of a library device, so it should be easy.

     

    When I draw the package (library editor), I can show Pads any way I like - eg. square pad with drill diam. larger than Pad edge, resulting in a 'Pad' with only the corners attached to a hole.

    This is an exaggeration of what I really want, but makes the point.

     

    When I Use the device on a .brd, the properties of the Pad are overridden.

     

    I've played with Restring values in DRC. I can grow the OD, but can't get it down to the size shown in the Library package.

     

    Is there something obvious I'm missing?

     

    An alternative approach would be a plated through hole with no ring at all (I'm not sure that's possible).

     

    cheers,

     

    ian

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/69238#69238/l/small-ring-pad--not-small-enough

     

     

    May I add some information about Restring? Hope this helps.....

     

     

      How to Define the Pad Diameter?

     

    Since EAGLE version 4.0 the default libraries contain only information

    about the drill diameter and the shape of a pad. The diameter value is

    set to auto, which is the same as 0, by default.

     

    What does this mean?

    The actual diameter will be calculated in the Layout Editor only. The

    calculation rule can be found in the Design Rules (menu Edit/Design

    Rules…) in the Restring tab. There you are allowed to define different

    calculation rules for Top, Bottom, and inner layers.

     

    How is it Calculated?

    The percentage, which is related to the drill diameter is used to

    calculate the width of the copper ring that is around the drilling.

    Default is 25%. A drill diameter of, for example, 0.032 inches results

    in a ring width of 0.008 inches.

    In the next step EAGLE checks if this value is within the given minimum

    and maximum boundaries. If so, the diameter of the pad results for our

    example in (2 * 0.008) + 0.032 = 0.048 inches.

    Let’s assume the minimum value is set to 0.010 inches. In this case the

    previously calculated value of 0.008 inches will be increased in order

    to accomplish this criteria to 0.010 inches. The resulting pad diameter

    will be 0.052 inches now.

    If the calculated value for the restring exceeds the value of the

    maximum limit it will be decreased to the maximum tolerated value.

    The minimum value represents in principle the Board house’s given

    production limits. This is the reason why it is forbidden to exceed the

    lower limits.

     

    What Happens if I Define a Diameter in the Package Editor?

    If you choose a value for the pad diameter in the Package Editor, EAGLE

    calculates again the width of the copper ring by the given percentage as

    soon as you add the part to the layout. The calculated value will be

    compared to the pre-defined one, resulting from the given diameter in

    the library. If the pre-defined value is smaller than the calculated

    value or the minimum limit is exceeded, the pad diameter will be increased.

    In the case of exceeding the maximum limit, EAGLE will tolerate this.

    The pad’s diameter won’t be reduced automatically!

     

    Changing the Design Rules affects the board immediately! Modify the

    settings for Restring and click the Apply button and you will see the

    result in the layout directly!

    Restring settings are valid for all the pads in the layout!

    It may happen that the pad diameter shown in the Package Editor or in

    the preview of the Device Editor or the Control Panel is not displayed

    exactly the same as it is in the Layout Editor because the Design Rules

    can be applied in the Layout Editor only!

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    On 08.02.2013 12:45, ian . wrote:

    Hi,

    I'm working on a project with 6.3 that was started in 6.2 - hopefully that won't make a difference.

     

    What I want to do is create a pad with a very small ring.

     

    In addition, I am trying to do this as part of a library device, so it should be easy.

     

    When I draw the package (library editor), I can show Pads any way I like - eg. square pad with drill diam. larger than Pad edge, resulting in a 'Pad' with only the corners attached to a hole.

    This is an exaggeration of what I really want, but makes the point.

     

    When I Use the device on a .brd, the properties of the Pad are overridden.

     

    I've played with Restring values in DRC. I can grow the OD, but can't get it down to the size shown in the Library package.

     

    Is there something obvious I'm missing?

     

    An alternative approach would be a plated through hole with no ring at all (I'm not sure that's possible).

     

    cheers,

     

    ian

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/69238#69238/l/small-ring-pad--not-small-enough

     

     

    May I add some information about Restring? Hope this helps.....

     

     

      How to Define the Pad Diameter?

     

    Since EAGLE version 4.0 the default libraries contain only information

    about the drill diameter and the shape of a pad. The diameter value is

    set to auto, which is the same as 0, by default.

     

    What does this mean?

    The actual diameter will be calculated in the Layout Editor only. The

    calculation rule can be found in the Design Rules (menu Edit/Design

    Rules…) in the Restring tab. There you are allowed to define different

    calculation rules for Top, Bottom, and inner layers.

     

    How is it Calculated?

    The percentage, which is related to the drill diameter is used to

    calculate the width of the copper ring that is around the drilling.

    Default is 25%. A drill diameter of, for example, 0.032 inches results

    in a ring width of 0.008 inches.

    In the next step EAGLE checks if this value is within the given minimum

    and maximum boundaries. If so, the diameter of the pad results for our

    example in (2 * 0.008) + 0.032 = 0.048 inches.

    Let’s assume the minimum value is set to 0.010 inches. In this case the

    previously calculated value of 0.008 inches will be increased in order

    to accomplish this criteria to 0.010 inches. The resulting pad diameter

    will be 0.052 inches now.

    If the calculated value for the restring exceeds the value of the

    maximum limit it will be decreased to the maximum tolerated value.

    The minimum value represents in principle the Board house’s given

    production limits. This is the reason why it is forbidden to exceed the

    lower limits.

     

    What Happens if I Define a Diameter in the Package Editor?

    If you choose a value for the pad diameter in the Package Editor, EAGLE

    calculates again the width of the copper ring by the given percentage as

    soon as you add the part to the layout. The calculated value will be

    compared to the pre-defined one, resulting from the given diameter in

    the library. If the pre-defined value is smaller than the calculated

    value or the minimum limit is exceeded, the pad diameter will be increased.

    In the case of exceeding the maximum limit, EAGLE will tolerate this.

    The pad’s diameter won’t be reduced automatically!

     

    Changing the Design Rules affects the board immediately! Modify the

    settings for Restring and click the Apply button and you will see the

    result in the layout directly!

    Restring settings are valid for all the pads in the layout!

    It may happen that the pad diameter shown in the Package Editor or in

    the preview of the Device Editor or the Control Panel is not displayed

    exactly the same as it is in the Layout Editor because the Design Rules

    can be applied in the Layout Editor only!

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/