Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Pin names on custom symbol
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 189 subscribers
  • Views 1968 views
  • Users 0 members are here
Related

Pin names on custom symbol

e14 Contributor
e14 Contributor over 13 years ago

Hello,

 

Is there an ASCII character to make certain characters in a symbol pin name subscript?  I am aware that the '!' character before and after text creates an overline for NOT inputs/outputs etc.

 

Also, how can you reduce the font size so that the opposite pin names do not overlap?  Currently it is set to 'Proportional' but I have also tried 'Fixed'.  Can the existing font size for pin names be changed?

 

The picture below shows the symbol I have attempted to create in Eagle with the actual manufacturers pin assignment diagram to the right of it.  I cannot reduce the font size of the (N.C.) Boost pin name on my Eagle part hence the symbol size has to be stretched horizontally to avoid overlap with the V+ text.  I also could not make +/- and V(OUT) subscript?

 

Thanks.

 

image

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 13 years ago

    On 18.04.2013 18:20, Gallium wrote:

    Hello,

     

    Is there an ASCII character to make certain characters in a symbol pin

    name subscript?  I am aware that the '!' character before and after text

    creates an overline for NOT inputs/outputs etc.

     

    Also, how can you reduce the font size so that the opposite pin names do

    not overlap?  Currently it is set to 'Proportional' but I have also

    tried 'Fixed'.  Can the existing font size for pin names be changed?

     

     

    No, the font size and position is fix and not user-definable.

    You could set Vsible = off and write the pin texts with the TEX command

    directly.

     

     

     

     

    The diagram below shows the symbol I have attempted to create in Eagle

    with the actual manufacturers pin assignment diagram to the right of

    it.  I cannot reduce the font size of the (N.C.) Boost pin name on my

    Eagle part hence the symbol size has to be stretched horizontally to

    avoid overlap with the V+ text.  I also could not make +/- and V(OUT)

    subscript?

     

    Thanks.

     

     

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/74426#74426

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to autodeskguest

     

    No, the font size and position is fix and not user-definable.

    You could set Vsible = off and write the pin texts with the TEX command

    directly.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

     

    Richard,

     

    Could you please explain what you mean by the above - How do I set Vsible = off?

     

    Also, is it possible to move the symbol pin text?  I would like to move POS and NEG in the coin cell battery holder symbol below?

     

    image

     

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bmoe
    0 bmoe over 13 years ago in reply to e14 Contributor

    Hi.

     

    The symbol pin text can not be moved but in the library symbol editor you can rightclick on your pin and chose properties, there you have an option called visible and if you set thet to OFF then you will not see either the pin name or number in your schematic.

    Instead you can use the text command to add text, like pin names wich you can change the size of, to your symbol, and place it whereever you want.

     

    /Matias

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bmoe
    0 bmoe over 13 years ago in reply to e14 Contributor

    Hi.

     

    The symbol pin text can not be moved but in the library symbol editor you can rightclick on your pin and chose properties, there you have an option called visible and if you set thet to OFF then you will not see either the pin name or number in your schematic.

    Instead you can use the text command to add text, like pin names wich you can change the size of, to your symbol, and place it whereever you want.

     

    /Matias