Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How to convert Eagle v4.0 files to 6.4?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 2317 views
  • Users 0 members are here
  • convert
  • version_update
  • 4.0_files
Related

How to convert Eagle v4.0 files to 6.4?

e14 Contributor
e14 Contributor over 13 years ago

I have some Eagle files (ver. 4.0.9, I think) that I'd like to be able to open (at least the schematics) in Eagle 6.4.0.  When I try opening them, I get the following error:

"Eagle for Mac OS X can't update file '<filename'>

(data structure is older than version 4.11"

 

I don't have ver. 5 or other versions of Eagle that might be able to open these files.

I can't find any ULP's or other ways for converting them, and the Eagle manual, update file, and readme doesn't tell me how to convert them either.

Suggestions?

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 13 years ago

    Am 06.05.2013 23:17, schrieb Bill Crosier:

    I have some Eagle files (ver. 4.0.9, I think) that I'd like to be able

    to open (at least the schematics) in Eagle 6.4.0.  When I try opening

    them, I get the following error:

    "Eagle for Mac OS X can't update file '<filename'>

    (data structure is older than version 4.11"

     

    [I might be wrong with the following sentences, but THINK that they're

    correct]

     

    As far as I know, EAGLE didn't EXIST for the Mac before version 4.11 (or

    something like that). Therefore, the CadSoft guys apparently didn't

    implement any reading algorithms for files before that version. Windows

    and Linux versions CAN read those files, though.

     

    It would be nice if the Windows and Mac algorithms could also be

    implemented for the Mac (by CadSoft), since there are obviously people

    who PREVIOUSLY used EAGLE under Windows/Linux (because it didn't exist

    for the Mac) and NOW use a Mac (because the like it) and want to read

    their old files. Having to install an OLD version on an additional

    NON-Mac and opening and saving the files there is quite definitely NOT

    the most user-friendly method.

     

    Implementing these reading algorithms shouldn't be difficult, because

    the Windows/Linux versions already HAVE them, and they have probably

    only been thrown out of the Mac version via some conditional compilation.

     

    Andreas Weidner

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to autodeskguest

    This solution worked great.  As a Mac user, I was able to open the older file and library versions with PC version 4.16 using "Save As".  After that they opened in Mac version 6.5 without any issues.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to autodeskguest

    This solution worked great.  As a Mac user, I was able to open the older file and library versions with PC version 4.16 using "Save As".  After that they opened in Mac version 6.5 without any issues.

     

    John