Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) ULP: Create reliable temp filename for scripts
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 19 replies
  • Subscribers 191 subscribers
  • Views 3038 views
  • Users 0 members are here
  • ulp
  • mac
Related

ULP: Create reliable temp filename for scripts

e14 Contributor
e14 Contributor over 13 years ago

Hello,

as far as I understand, the only way to manipulate the data structure of either an eagle schematic, board or library through an ULP is to collect the necessary commands in a text file and execute it using exit ("script <filename>"). This method works as long as there is a suitable filename available that is writeable. On a unix system, this would be somewhere in /tmp, on windows, this would be some other location. I have failed so far to find a way to create a temporary filename that works across all supported operating systems. I suggest to add a function to create a temporary path for exactly that purpose and to document it together with the whole approach of collecting commands to manipulate the data structure in a script and execute that script after the ULP is finished. This would have the other advantage that the script could get deleted after execution because it is intended for a single execution anyway.

 

What do you think about this? Does anyone has a realiable solution to create a temporary filename? I think the currently most used approach is to place the script into the same directory as the currently edited schematic or library. This works because the user usually has the rights to write to the directory of the currently edited file. But I think this is a hack because the file remains after execution and does not belong there. Another interesting idea would be to have a magic filename, for example ":memory" so the commands get stored somewhere in memory, exeuted and never become an object in the users filesystem.

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    0 dukepro over 13 years ago

    On 06/20/2013 09:06 AM, Axel Jäger wrote:

    Hello,

    as far as I understand, the only way to manipulate the data structure of

    either an eagle schematic, board or library through an ULP is to collect

    the necessary commands in a text file and execute it using exit ("script

    <filename>").

     

    Axel,

     

    Rather than collecting commands into a file, collect them into a string

    then pass the string as the single argument to exit().

     

        string cmd = "";

     

        cmd += "display all;\n";    // display all layers

        cmd += "group all;\n";      // Group all objects

        cmd += "lock (CS> 0 0);\n"; // Unlock everything.

        cmd += "display last;\n";   // restore the original display

        ... add more useful commands to cmd

        exit(cmd);

     

    No files are used here.

     

    HTH,

        - Chuck

     

     

    Attachments:
    2234.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to dukepro

    Chuck: THIS is the solution, many thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 13 years ago in reply to e14 Contributor

    Axel Jäger wrote:

    Chuck: THIS is the solution, many thanks.

     

    --

     

    Chuck's solution is used often but is slow when you perform many cmd +=

    Concatenating strings in a ULP is slow.

     

    When that becomes and issue you can have your ULP create your script file in

    the directory of the current  editor file you have open. You  know you can

    write to that place.

    You create the file using  open ("text file",wtD) so that that file is

    deleted when Eagle is closed. Hence the file is temporary.

     

    I think that covers your needs

     

    Warren

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 13 years ago in reply to CSWalt

    Walter Spermann wrote on Thu, 27 June 2013 05:40

    Hi,

     

    ]

    if you have a loop that does a concatenation in each step like

    "

    string Result;

    string Lines[]; // say 100000 lines filled with some strings

    for (int i=0; i<100000; ++i)

       Result += Lines[i];

    "

    then in each step a reallocation occurs for Result which takes time.

    In that case strjoin is much better:

    "

    Result = strjoin(Lines,'');

    "

    strjoin does the whole thing in one step, only one reallocation and

    copy.

    Hope this makes it clearer.

     

     

    Thanks for the information Walter.

     

    To all.

    I have had a further play. I wondered how the final string size affected

    performance. I found once the size exceeded 132KB the times increased

    dramatically. The graph headed for the heavens.

    That size string would not be common so is probably not relevant

     

    sprintf() has a far more dramatic effect. The attached ULP illustrates

    this.

    So, in some ULPs it would be worth using sprintf() sparingly.

     

    I noticed when running the ULP that the reported times varied quite a bit

    with either of the top two sprintf techniques  being the faster. The string

    size remained the same so I can only imagine there is contention for

    resources when this is observed. 

     

    Regards

    Warren

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    Attachments:
    Avoidsprintf.ulp.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 13 years ago in reply to CSWalt

    Walter Spermann wrote on Thu, 27 June 2013 05:40

    Hi,

     

    ]

    if you have a loop that does a concatenation in each step like

    "

    string Result;

    string Lines[]; // say 100000 lines filled with some strings

    for (int i=0; i<100000; ++i)

       Result += Lines[i];

    "

    then in each step a reallocation occurs for Result which takes time.

    In that case strjoin is much better:

    "

    Result = strjoin(Lines,'');

    "

    strjoin does the whole thing in one step, only one reallocation and

    copy.

    Hope this makes it clearer.

     

     

    Thanks for the information Walter.

     

    To all.

    I have had a further play. I wondered how the final string size affected

    performance. I found once the size exceeded 132KB the times increased

    dramatically. The graph headed for the heavens.

    That size string would not be common so is probably not relevant

     

    sprintf() has a far more dramatic effect. The attached ULP illustrates

    this.

    So, in some ULPs it would be worth using sprintf() sparingly.

     

    I noticed when running the ULP that the reported times varied quite a bit

    with either of the top two sprintf techniques  being the faster. The string

    size remained the same so I can only imagine there is contention for

    resources when this is observed. 

     

    Regards

    Warren

     

     

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    Attachments:
    Avoidsprintf.ulp.zip