EAGLE User Support (English) Transfer an Eagle project
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
  • State Not Answered
  • Replies 2 replies
  • Subscribers 177 subscribers
  • Views 2249 views
  • Users 0 members are here
  • project
  • transfer
Related

Transfer an Eagle project

Former Member
Former Member over 12 years ago

Hello,

 

Could someone tell me how I can transfer an Eagle project that I have created on a computer (including libraries) to another computer running Eagle?

 

Thanks.

  • Sign in to reply
  • Cancel
  • shabaz
    0 shabaz over 12 years ago

    Hi,

     

    You can copy across the entire folder in which you have created your project, plus any folder in which you have any custom libraries. After that, you will see it in your EAGLE Control Panel, when you start up EAGLE on your target computer assuming it is set up with the folder paths.

    Typically, I set the EAGLE Control Panel -> Options -> Directories to have my custom folder paths as well as the default paths.

    So, for example, the 'Libraries' setting could be $EAGLEDIR\lbr;C:\projects\EAGLE_FILES

    and so on for the other settings.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago

    Am 10.06.2013 13:40, schrieb Gallium:

    Could someone tell me how I can transfer an Eagle project that I have

    created on a computer (including libraries) to another computer running

    Eagle?

     

    You ONLY need to copy the BRD and SCH fils. All necessary library

    information etc. is already included in these.

     

    All other files are NOT necessary, but of course you CAN decide to copy

    them, too, e.g.:

      - The EPF file (if available) contains EAGLE program settings for

        your project. Mind that this might contain information about

        folders that are perhaps not available on the other PC.

      - The used libraries. Useful if you want to make extensive changes

        to a project that contains self-made libraries.

     

    Andreas Weidner