EAGLE User Support (English) Eagle PCB check
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
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 1000 views
  • Users 0 members are here
Related

Eagle PCB check

anshulsanam
anshulsanam over 12 years ago

I'm a beginner in eagle and I designed a PCB and I am ready to send it off to the PCB fab house.

but I need to make sure the board is gonna work cause I dont wanna spend 40 dollars on the PCB and have it short or not work.

 

So could you guys check the schematic and board file.

http://www.fast-files.com/getfile.aspx?file=63502                   -            schematic

http://www.fast-files.com/getfile.aspx?file=63503                   -             board file

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    anshul sanam wrote:

    I'm a beginner in eagle and I designed a PCB and I am ready to send it

    off to the PCB fab house.

    but I need to make sure the board is gonna work cause I dont wanna

    spend 40 dollars on the PCB and have it short or not work.

     

     

    Things I would change

    1) The tPlace font is Proportional, make it Vector so you get what you see.

    2) Move the text off the pads, The board house will chop the characters to

    bits to satisfy this. Best you move the text so its readable when the board

    comes back.

    3) Text like R4 will not come back readable as it is to thin. Currently the

    characters are 16mil high and the strokes of the chars  are 8% of that,

    about 1.2mil. Your board house likely has a >5mil  recomendation  for

    printed objects

    4) All the servo connectors have power connections with only three spokes of

    the thermal connected. with some shifting of nearby traces they could have 4

    spokes giving greater strength and current capability.

    5) Reduce the wire size for the polygon pours to 10mil, It gets rid of a few

    unclosed regions.

    6) Move R8 further left, its quite near the board edge. Align it with R5

    pad.

     

    Last thing. When you generate your gerbers, view them in a gerber viewer

    before you send them off.

     

    HTH

    Warren

     

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • anshulsanam
    0 anshulsanam over 12 years ago in reply to autodeskguest

    do you think the voltage dividers for the sensors are proper

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • anshulsanam
    0 anshulsanam over 12 years ago in reply to autodeskguest

    do you think the voltage dividers for the sensors are proper