EAGLE User Support (English) Eagle PCB check
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
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 179 subscribers
  • Views 997 views
  • Users 0 members are here
Related

Eagle PCB check

anshulsanam
anshulsanam over 12 years ago

I'm a beginner in eagle and I designed a PCB and I am ready to send it off to the PCB fab house.

but I need to make sure the board is gonna work cause I dont wanna spend 40 dollars on the PCB and have it short or not work.

 

So could you guys check the schematic and board file.

http://www.fast-files.com/getfile.aspx?file=63502                   -            schematic

http://www.fast-files.com/getfile.aspx?file=63503                   -             board file

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    anshul sanam wrote:

    I'm a beginner in eagle and I designed a PCB and I am ready to send it

    off to the PCB fab house.

    but I need to make sure the board is gonna work cause I dont wanna

    spend 40 dollars on the PCB and have it short or not work.

     

     

    Things I would change

    1) The tPlace font is Proportional, make it Vector so you get what you see.

    2) Move the text off the pads, The board house will chop the characters to

    bits to satisfy this. Best you move the text so its readable when the board

    comes back.

    3) Text like R4 will not come back readable as it is to thin. Currently the

    characters are 16mil high and the strokes of the chars  are 8% of that,

    about 1.2mil. Your board house likely has a >5mil  recomendation  for

    printed objects

    4) All the servo connectors have power connections with only three spokes of

    the thermal connected. with some shifting of nearby traces they could have 4

    spokes giving greater strength and current capability.

    5) Reduce the wire size for the polygon pours to 10mil, It gets rid of a few

    unclosed regions.

    6) Move R8 further left, its quite near the board edge. Align it with R5

    pad.

     

    Last thing. When you generate your gerbers, view them in a gerber viewer

    before you send them off.

     

    HTH

    Warren

     

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • anshulsanam
    0 anshulsanam over 12 years ago in reply to autodeskguest

    thanks a lot for the suggestions i didnt understand how you could get 4 thermal spokes do i just move nearby traces further away, also do you think everything else is fine, and is there a good chance I will get it working after i get the real PCB back

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to anshulsanam

    anshul sanam wrote:

    thanks a lot for the suggestions i didnt understand how you could get

    4 thermal spokes do i just move nearby traces further away, also do

    you think everything else is fine, and is there a good chance I will

    get it working after i get the real PCB back

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/79921#79921

     

    Hi

    The thermal spokes are formed when the polygon pour fills. Currently the

    pour, made with the same width wires as you define the polygon outline with

    (your 10 or 16 mil wires), cannot fit all the way around certain places so

    you have to make it possible for them to get in there. You need to move

    traces, or other objects that  require clearances, out of the way for that

    to happen. From what I could see that would be an easy job.

     

    I can't comment on whether every thing else is fine or that it will all work

    when the PCB comes back, that depends on your electrical design. If the

    schematic was wrong then the circuit may not work. Ensure you run an ERC

    check  That should pick up any missing connections.

    What I'm helping you here with is applying better PCB design practice,

    hence reducing the chances that the PCB will contribute to any problem

    initially or during its life.

    The end goal for any PCB is one that is electrically correct and strong so

    that it resists the abuse it will be subjected to during assembly

    (soldering) and during it's life.

     

    All the best

    Warren

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anshulsanam
    0 anshulsanam over 12 years ago in reply to autodeskguest

    I have made a final revision which Im confident on. I just want to know if you guys think it correct

     

    schematic - http://www.mediafire.com/download/qq1kudnnalgebel/anshuluinonewnew.sch

     

    board - http://www.mediafire.com/download/2ld2l1ijhulftk7/anshuluinonewnew.brd

     

    thanks image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fritzz
    0 fritzz over 12 years ago in reply to anshulsanam

    I get

     

    Loading C:/Program Files/EAGLE-6.2.0/projects/someone elses/anshuluinonewnew.brd ... 

    Warning(s):

    line 356: unknown attribute 'name' in tag <designrules>

     

    when I try to load this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fritzz
    0 fritzz over 12 years ago in reply to fritzz

    Text of that LED is overwriitne by another text.

    Maybe add a bypass cap on chip's VCC also?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • fritzz
    0 fritzz over 12 years ago in reply to fritzz

    Text of that LED is overwriitne by another text.

    Maybe add a bypass cap on chip's VCC also?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • anshulsanam
    0 anshulsanam over 12 years ago in reply to fritzz

    oh ok thanks for the help what value cap should i use and does everything else look correct

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fritzz
    0 fritzz over 12 years ago in reply to anshulsanam

    I didn't look at it long enough to say that's all that might be an issue.

     

    .1uf