Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Connecting pins without wire
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 190 subscribers
  • Views 2118 views
  • Users 0 members are here
  • eagle
  • pins
  • wires
  • schematic
Related

Connecting pins without wire

bazz
bazz over 13 years ago

If you look at the attached pdf file, it is a schematic, where the IC pins are not all connected explicitly with wires. However, the pins are still shown to make connections to the connectors. How can I achieve the same look and feel with Eagle Cad?

Attachments:
imagefx2_v200.pdf
  • Sign in to reply
  • Cancel
  • dukepro
    0 dukepro over 13 years ago in reply to bazz

    On 07/12/2013 08:02 AM, Michael Bazzinotti wrote:

    Ok I figured it out. You can use the Label command after the nets are

    connected, click the net you want the label to float around, and you can

    adjust its angle etc. is there a faster way to adjust its angle than

    having to move the mouse to the top of the window??

     

    Sure.  While you're positioning the label, right click.  That should

    rotate CCW 90 degrees per click.  If you need an oddball angle, click

    right on the label and select properties, then enter the desired angle.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bazz
    0 bazz over 13 years ago

    Ok I figured it out. You can use the Label command after the nets are connected, click the net you want the label to float around, and you can adjust its angle etc. is there a faster way to adjust its angle than having to move the mouse to the top of the window??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bazz
    0 bazz over 13 years ago in reply to fritzz

    That helped me 50%. You helped me connect the signals, that's great. However, can I get the Text labels to correlate? Without text, it will be impossible to read the schematic without analysis in software. If you look at the PDF I attached in the original post, you see that the name of the chip pin is reflected over the net coming from the connector. I would like the name of the pin to appear in this way when I connect the signals.

     

    It would be great to have this happen automatically instead of having to manually use the Text command for every signal on a 128-pin chip image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fritzz
    0 fritzz over 13 years ago

    Draw two nets. Then give them the same name.

     

    Is that what you are after?

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer