EAGLE User Support (English) USB 2.0 - Mandatory 4 layers and impedance matching?
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
  • Replies 6 replies
  • Subscribers 180 subscribers
  • Views 1000 views
  • Users 0 members are here
Related

USB 2.0 - Mandatory 4 layers and impedance matching?

autodeskguest
autodeskguest over 17 years ago

I have brougth this topic up again, because I have some doubts: people

usually say that it is mandatory to use a 4-layered boards with impedance

matching when you have a USB 2.0 circuit on board. But my question is: even

if I know that the circuit won´t reach 20Mbps tops (very far from 480Mbps of

USB 2.0) is it really mandatory to have a 4-layers board? And the impedance?

What if I make the trace as short as possible, from the connector to the IC?

 

Thanks

 

Thiago

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 17 years ago

    Well then, just breadboard the thing and see if it works!  Good luck!

     

     

    "Thiago" <thiago_hr@yahoo.com.br> wrote in message

    news:gfdfs5$9po$1@cheetah.cadsoft.de...

     

    Yes, I am aware of this DOC, but this is exactly what I wanted to avoid: 4

    layers and impedance matching calculations.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 17 years ago

    Well then, just breadboard the thing and see if it works!  Good luck!

     

     

    "Thiago" <thiago_hr@yahoo.com.br> wrote in message

    news:gfdfs5$9po$1@cheetah.cadsoft.de...

     

    Yes, I am aware of this DOC, but this is exactly what I wanted to avoid: 4

    layers and impedance matching calculations.