EAGLE User Support (English) restrict not respected
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
  • Replies 4 replies
  • Subscribers 178 subscribers
  • Views 747 views
  • Users 0 members are here
Related

restrict not respected

autodeskguest
autodeskguest over 17 years ago

I have a 4 layer board that will have a large half inch hole drilled

through it for connector/wire pass through.  I have not placed a 'hole'

there because it is too large for the board house' I'll drill it myself.

  I've drawn circles in the tRestrict, bRestrict and vRestrict layers to

keep traces out of the hole area.  The GND layer is a pologon named GND

and grounds route around the hole fine.

 

The first few times I auto routed the board the restrict circles were

respected - no traces were placed inside them.  After working with the

board for a while the auto router now places traces and vias inside the

restrict circles.

 

I haven't changed the circles or layer definitions, just added parts and

moved things around.  It's a pretty dense board and routing is done in

top, bottom and vcc layers to get everything connected.

 

So I'm guessing either I've messed up some other parameter that turns

off the effect of the restrict circles or perhaps the board cannot be

routed without violating them??

Any thoughts appreciated.

 

Jim

 

Jim White

jim@coloradosatelite.com

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 17 years ago

    Jim White schrieb:

    I've drawn zero width circles in top, bottom, vcc (used for routing) and

    GND. That prevents routing in the circle in all four layers.  However

    drawing a zero width circle in the GND layer which is filled with a

    polygon ground plane results in that hole (circle) being filled with

    copper.

    So the question now is how to make a large hole in a polygon ground plane?

     

    Jim

     

     

    Why not draw a circle with a very fine width of for example

    0.001 inch in the inner layer? The polygon keeps its clearance

    to the circumference and the inner part will be kept copper

    free, if the polygon parameter "orphans" is set "off".

     

    Basically bigger holes are not drilled but milled. You could

    draw the same circle in the Milling layer (46) and tell the

    board manufacturer that in layer 46 are milling contours to

    be taken in consideration.

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 17 years ago

    Jim White schrieb:

    I've drawn zero width circles in top, bottom, vcc (used for routing) and

    GND. That prevents routing in the circle in all four layers.  However

    drawing a zero width circle in the GND layer which is filled with a

    polygon ground plane results in that hole (circle) being filled with

    copper.

    So the question now is how to make a large hole in a polygon ground plane?

     

    Jim

     

     

    Why not draw a circle with a very fine width of for example

    0.001 inch in the inner layer? The polygon keeps its clearance

    to the circumference and the inner part will be kept copper

    free, if the polygon parameter "orphans" is set "off".

     

    Basically bigger holes are not drilled but milled. You could

    draw the same circle in the Milling layer (46) and tell the

    board manufacturer that in layer 46 are milling contours to

    be taken in consideration.

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm