EAGLE User Support (English) restrict not respected
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
  • Replies 4 replies
  • Subscribers 178 subscribers
  • Views 746 views
  • Users 0 members are here
Related

restrict not respected

autodeskguest
autodeskguest over 17 years ago

I have a 4 layer board that will have a large half inch hole drilled

through it for connector/wire pass through.  I have not placed a 'hole'

there because it is too large for the board house' I'll drill it myself.

  I've drawn circles in the tRestrict, bRestrict and vRestrict layers to

keep traces out of the hole area.  The GND layer is a pologon named GND

and grounds route around the hole fine.

 

The first few times I auto routed the board the restrict circles were

respected - no traces were placed inside them.  After working with the

board for a while the auto router now places traces and vias inside the

restrict circles.

 

I haven't changed the circles or layer definitions, just added parts and

moved things around.  It's a pretty dense board and routing is done in

top, bottom and vcc layers to get everything connected.

 

So I'm guessing either I've messed up some other parameter that turns

off the effect of the restrict circles or perhaps the board cannot be

routed without violating them??

Any thoughts appreciated.

 

Jim

 

Jim White

jim@coloradosatelite.com

 

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 17 years ago

    Jim White schrieb:

    I have a 4 layer board that will have a large half inch hole drilled

    through it for connector/wire pass through.  I have not placed a 'hole'

    there because it is too large for the board house' I'll drill it myself.

    I've drawn circles in the tRestrict, bRestrict and vRestrict layers to

    keep traces out of the hole area.  The GND layer is a pologon named GND

    and grounds route around the hole fine.

     

    The first few times I auto routed the board the restrict circles were

    respected - no traces were placed inside them.  After working with the

    board for a while the auto router now places traces and vias inside the

    restrict circles.

     

    I haven't changed the circles or layer definitions, just added parts and

    moved things around.  It's a pretty dense board and routing is done in

    top, bottom and vcc layers to get everything connected.

     

    So I'm guessing either I've messed up some other parameter that turns

    off the effect of the restrict circles or perhaps the board cannot be

    routed without violating them??

    Any thoughts appreciated.

     

    Jim

     

    Jim White

    jim@coloradosatelite.com

     

     

    Did you draw the circles in t/b/vRestrict with a width of 0

    for filled circles?

     

    And what about the inner layers? t/bRestrict only works for the

    outer layers? Did you draw also circles in the inner layers?

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    I've drawn zero width circles in top, bottom, vcc (used for routing) and

    GND. That prevents routing in the circle in all four layers.  However

    drawing a zero width circle in the GND layer which is filled with a

    polygon ground plane results in that hole (circle) being filled with copper.

    So the question now is how to make a large hole in a polygon ground plane?

     

    Jim

     

     

    Richard Hammerl wrote:

    Jim White schrieb:

    I have a 4 layer board that will have a large half inch hole drilled

    through it for connector/wire pass through.  I have not placed a 'hole'

    there because it is too large for the board house' I'll drill it myself.

    I've drawn circles in the tRestrict, bRestrict and vRestrict layers to

    keep traces out of the hole area.  The GND layer is a pologon named GND

    and grounds route around the hole fine.

     

    The first few times I auto routed the board the restrict circles were

    respected - no traces were placed inside them.  After working with the

    board for a while the auto router now places traces and vias inside the

    restrict circles.

     

    I haven't changed the circles or layer definitions, just added parts and

    moved things around.  It's a pretty dense board and routing is done in

    top, bottom and vcc layers to get everything connected.

     

    So I'm guessing either I've messed up some other parameter that turns

    off the effect of the restrict circles or perhaps the board cannot be

    routed without violating them??

    Any thoughts appreciated.

     

    Jim

     

    Jim White

    jim@coloradosatelite.com

     

    Did you draw the circles in t/b/vRestrict with a width of 0

    for filled circles?

     

    And what about the inner layers? t/bRestrict only works for the

    outer layers? Did you draw also circles in the inner layers?

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 17 years ago

    Jim White schrieb:

    I've drawn zero width circles in top, bottom, vcc (used for routing) and

    GND. That prevents routing in the circle in all four layers.  However

    drawing a zero width circle in the GND layer which is filled with a

    polygon ground plane results in that hole (circle) being filled with

    copper.

    So the question now is how to make a large hole in a polygon ground plane?

     

    Jim

     

     

    Why not draw a circle with a very fine width of for example

    0.001 inch in the inner layer? The polygon keeps its clearance

    to the circumference and the inner part will be kept copper

    free, if the polygon parameter "orphans" is set "off".

     

    Basically bigger holes are not drilled but milled. You could

    draw the same circle in the Milling layer (46) and tell the

    board manufacturer that in layer 46 are milling contours to

    be taken in consideration.

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    The way I worked around this was to place z width circles in trestrict,

    vrestrict and brestrict. Then I put a circle in my ground plane, which

    was filled. Then routed the board and deleted that circle in the ground

    plane.  That gets me a nice clean spot in the board where I can drill

    the hole, or use a Dremel tool to mill it out.

    Jim

     

    Richard Hammerl wrote:

    Jim White schrieb:

    I've drawn zero width circles in top, bottom, vcc (used for routing) and

    GND. That prevents routing in the circle in all four layers.  However

    drawing a zero width circle in the GND layer which is filled with a

    polygon ground plane results in that hole (circle) being filled with

    copper.

    So the question now is how to make a large hole in a polygon ground plane?

     

    Jim

     

    Why not draw a circle with a very fine width of for example

    0.001 inch in the inner layer? The polygon keeps its clearance

    to the circumference and the inner part will be kept copper

    free, if the polygon parameter "orphans" is set "off".

     

    Basically bigger holes are not drilled but milled. You could

    draw the same circle in the Milling layer (46) and tell the

    board manufacturer that in layer 46 are milling contours to

    be taken in consideration.