EAGLE User Support (English) Power and Supply Pin Use on Schematics
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
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 181 subscribers
  • Views 5886 views
  • Users 0 members are here
  • pins
  • supply
  • connections
  • power
Related

Power and Supply Pin Use on Schematics

Former Member
Former Member over 12 years ago

I've created a schematic design for a digital circuit with an isolated RS422 section. I'm using an isolating power supply for the transceivers and bringing the data lines onto the main board using an optoisolator. From that point, the rest of the board has common power and grounds. I'm using polygons with different names for GND on each section.

 

I'm running into 2 distinct problems.

1) I need to keep the isolated VCC and GND nets separated on the schematic. I'm having some sucess with this as I am using different net names (i.e. GND and -VOUT)

2) Power and Supply pins are more challenging. Some IC's have VCC, others VDD. The isolated section I've given the net name of +VOUT. All are at +5v.

 

When I run ERC, I get warnings of interconnected nets. I believe I'm using Power and Supply pins incorrectly. Simple case - how do I properly connect +5v to VCC and to VDD on the same net?

 

imageimageimage

Slight mess! Yes, VDD has no net as it will generate more errors if I connect it to +5v.

 

I appreciate your time and suggestions!

 

Warm regards.

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 09/30/2013 11:27 AM, David Kanazawa wrote:

    When I run ERC, I get warnings of interconnected nets. I believe I'm

    using Power and Supply pins incorrectly. Simple case - how do I properly

    connect +5v to VCC and to VDD on the same net?

    It is a warning. Either ignore it or fix the component to match your

    power and ground names. This is a check that helps simple circuits of

    beginners and a nuance with complex circuits.

    Paul

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 09/30/2013 11:27 AM, David Kanazawa wrote:

    When I run ERC, I get warnings of interconnected nets. I believe I'm

    using Power and Supply pins incorrectly. Simple case - how do I properly

    connect +5v to VCC and to VDD on the same net?

    It is a warning. Either ignore it or fix the component to match your

    power and ground names. This is a check that helps simple circuits of

    beginners and a nuance with complex circuits.

    Paul