Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Power and Supply Pin Use on Schematics
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 189 subscribers
  • Views 6231 views
  • Users 0 members are here
  • pins
  • supply
  • connections
  • power
Related

Power and Supply Pin Use on Schematics

e14 Contributor
e14 Contributor over 12 years ago

I've created a schematic design for a digital circuit with an isolated RS422 section. I'm using an isolating power supply for the transceivers and bringing the data lines onto the main board using an optoisolator. From that point, the rest of the board has common power and grounds. I'm using polygons with different names for GND on each section.

 

I'm running into 2 distinct problems.

1) I need to keep the isolated VCC and GND nets separated on the schematic. I'm having some sucess with this as I am using different net names (i.e. GND and -VOUT)

2) Power and Supply pins are more challenging. Some IC's have VCC, others VDD. The isolated section I've given the net name of +VOUT. All are at +5v.

 

When I run ERC, I get warnings of interconnected nets. I believe I'm using Power and Supply pins incorrectly. Simple case - how do I properly connect +5v to VCC and to VDD on the same net?

 

imageimageimage

Slight mess! Yes, VDD has no net as it will generate more errors if I connect it to +5v.

 

I appreciate your time and suggestions!

 

Warm regards.

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    0 dukepro over 12 years ago

    On 09/30/2013 11:27 AM, David Kanazawa wrote:

    ...

    I'm running into 2 distinct problems.

    1) I need to keep the isolated VCC and GND nets separated on the

    schematic. I'm having some sucess with this as I am using different net

    names (i.e. GND and -VOUT)

     

    Use the supply symbols in supply.lbr or supply2.lbr for each of your

    different nets.  i.e. GND, GND1, GND2, etc.

    Eagle will treat these, as it should, as separate nets.  To tie them

    together, use the SHORT device in the attached shorts.lbr.  This is

    merely two pads that overlap each other.  This will produce a DRC error,

    but it can be approved to prevent from being a nuisance.

     

    2) Power and Supply pins are more challenging. Some IC's have VCC,

    others VDD. The isolated section I've given the net name of +VOUT. All

    are at +5v.

     

    You can use the supply symbol +5V from the supply2 library to name the

    net (it conveys more information to the reader).

    When I run ERC, I get warnings of interconnected nets. I believe I'm

    using Power and Supply pins incorrectly. Simple case - how do I properly

    connect +5v to VCC and to VDD on the same net?

    ERC warnings of the type "VCC connected to +5V" can be approved.  All it

    means is that the name of the power pin does not match the name of the

    net to which it's connected.

     

    If you want to connect separate nets, use the SHORT device.

     

    I do this quite often to separate different grounds such as analog

    ground, a noisy high-power ground, and a logic ground.  I want to tie

    them all together eventually, but keep them separate as long as

    possible.  So all the shorts are placed close to the battery connector.

    Since it's an on-board component, I take all shorts out of the BOM.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dukepro
    0 dukepro over 12 years ago

    On 09/30/2013 11:27 AM, David Kanazawa wrote:

    ...

    I'm running into 2 distinct problems.

    1) I need to keep the isolated VCC and GND nets separated on the

    schematic. I'm having some sucess with this as I am using different net

    names (i.e. GND and -VOUT)

     

    Use the supply symbols in supply.lbr or supply2.lbr for each of your

    different nets.  i.e. GND, GND1, GND2, etc.

    Eagle will treat these, as it should, as separate nets.  To tie them

    together, use the SHORT device in the attached shorts.lbr.  This is

    merely two pads that overlap each other.  This will produce a DRC error,

    but it can be approved to prevent from being a nuisance.

     

    2) Power and Supply pins are more challenging. Some IC's have VCC,

    others VDD. The isolated section I've given the net name of +VOUT. All

    are at +5v.

     

    You can use the supply symbol +5V from the supply2 library to name the

    net (it conveys more information to the reader).

    When I run ERC, I get warnings of interconnected nets. I believe I'm

    using Power and Supply pins incorrectly. Simple case - how do I properly

    connect +5v to VCC and to VDD on the same net?

    ERC warnings of the type "VCC connected to +5V" can be approved.  All it

    means is that the name of the power pin does not match the name of the

    net to which it's connected.

     

    If you want to connect separate nets, use the SHORT device.

     

    I do this quite often to separate different grounds such as analog

    ground, a noisy high-power ground, and a logic ground.  I want to tie

    them all together eventually, but keep them separate as long as

    possible.  So all the shorts are placed close to the battery connector.

    Since it's an on-board component, I take all shorts out of the BOM.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to dukepro

    Paul and Chuck,

     

    Thanks very much for taking the time to help (re)explain this issue. It's very helpful to have the concrete examples of devices, the error messages and result of "approving" errors. It would not have occurred to me to search for the SHORT device, so that was particularly useful. I'll give this a go and hopefully it will allow me to complete this section of schematic layout. Nice touch on removing the SHORT from the BOM.

     

    One side note - I'm not clear on why it's necessary to even have the supply and power connections laid out. Is it for clarity of which voltage is being applied to a particular net such as defining the VCC voltage?

     

    And on to the next topic - "Polygons May Have Fallen Apart".

     

    Thank you for helping me understand how to use these tools!

     

    David K.