Hi,
When i run erc command i get this error. I checked the SPI-SDI net but
could not see anything wrong. So, What does this error mean ? Is it a
critical one ?
Best regards,
Firat
Hi,
When i run erc command i get this error. I checked the SPI-SDI net but
could not see anything wrong. So, What does this error mean ? Is it a
critical one ?
Best regards,
Firat
Joern Paschedag wrote:
Firat Kocak schrieb:
Hi,
When i run erc command i get this error. I checked the SPI-SDI net but
could not see anything wrong. So, What does this error mean ? Is it a
critical one ?
Best regards,
Firat
It normally is critical because it means that two outputs are connected
together. This can mean i.e. that one output provides a high supply
voltge and the other one the ground. Result will be a nice smell of Amps.
Only open collector outputs may be connected together and perhaps
tristate outputs with appropriate control.
Maybe just the direction of a pin is wrong in a library.
Hi,
Thanks for the reply. I will check it again. But the SPI-SDI net is
connected to the SDO pins of the SPI devices and SDI pin of the mcu. I
would rather delete SPI-SDI and create it again.
Regards,
Firat
Joern Paschedag wrote:
Firat Kocak schrieb:
Hi,
When i run erc command i get this error. I checked the SPI-SDI net but
could not see anything wrong. So, What does this error mean ? Is it a
critical one ?
Best regards,
Firat
It normally is critical because it means that two outputs are connected
together. This can mean i.e. that one output provides a high supply
voltge and the other one the ground. Result will be a nice smell of Amps.
Only open collector outputs may be connected together and perhaps
tristate outputs with appropriate control.
Maybe just the direction of a pin is wrong in a library.
Hi,
Thanks for the reply. I will check it again. But the SPI-SDI net is
connected to the SDO pins of the SPI devices and SDI pin of the mcu. I
would rather delete SPI-SDI and create it again.
Regards,
Firat