EAGLE User Support (English) What does "ERROR: 2 OUTPUT Pins on net SPI-SDI" mean ?
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
  • Replies 4 replies
  • Subscribers 178 subscribers
  • Views 475 views
  • Users 0 members are here
Related

What does "ERROR: 2 OUTPUT Pins on net SPI-SDI" mean ?

firatkocak
firatkocak over 17 years ago

Hi,

 

When i run erc command i get this error. I checked the SPI-SDI net but

could not see anything wrong. So, What does this error mean ? Is it a

critical one ?

 

Best regards,

 

Firat

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Firat Kocak schrieb:

    Hi,

     

    When i run erc command i get this error. I checked the SPI-SDI net but

    could not see anything wrong. So, What does this error mean ? Is it a

    critical one ?

     

    Best regards,

     

    Firat

     

    It normally is critical because it means that two outputs are connected

    together. This can mean i.e. that one output provides a high supply

    voltge and the other one the ground. Result will be a nice smell of Amps.

    Only open collector outputs may be connected together and perhaps

    tristate outputs with appropriate control.

    Maybe just the direction of a pin is wrong in a library.

     

    --

    Gruß / regards

     

    Jörn

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • firatkocak
    firatkocak over 17 years ago

    Joern Paschedag wrote:

    Firat Kocak schrieb:

    Hi,

     

    When i run erc command i get this error. I checked the SPI-SDI net but

    could not see anything wrong. So, What does this error mean ? Is it a

    critical one ?

     

    Best regards,

     

    Firat

     

    It normally is critical because it means that two outputs are connected

    together. This can mean i.e. that one output provides a high supply

    voltge and the other one the ground. Result will be a nice smell of Amps.

    Only open collector outputs may be connected together and perhaps

    tristate outputs with appropriate control.

    Maybe just the direction of a pin is wrong in a library.

     

     

    Hi,

     

    Thanks for the reply. I will check it again. But the SPI-SDI net is

    connected to the SDO pins of the SPI devices and SDI pin of the mcu. I

    would rather delete SPI-SDI and create it again.

     

    Regards,

     

    Firat

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Firat Kocak wrote:

    Joern Paschedag wrote:

    Firat Kocak schrieb:

    Hi,

     

    When i run erc command i get this error. I checked the SPI-SDI net

    but could not see anything wrong. So, What does this error mean ?

    Is it a critical one ?

     

    Best regards,

     

    Firat

     

    It normally is critical because it means that two outputs are

    connected together. This can mean i.e. that one output provides a

    high supply voltge and the other one the ground. Result will be a

    nice smell of Amps. Only open collector outputs may be connected

    together and perhaps tristate outputs with appropriate control.

    Maybe just the direction of a pin is wrong in a library.

     

     

    Hi,

     

    Thanks for the reply. I will check it again. But the SPI-SDI net is

    connected to the SDO pins of the SPI devices and SDI pin of the mcu. I

    would rather delete SPI-SDI and create it again.

     

    As Joern suggested, check the direction of the pins in the library where

    each part comes from.  Maybe the SDI pin of the MCU is not defined as an

    input.

     

    --

    Bert Menkveld

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • firatkocak
    firatkocak over 17 years ago

    Bert Menkveld wrote:

    Firat Kocak wrote:

    Joern Paschedag wrote:

    Firat Kocak schrieb:

    Hi,

     

    When i run erc command i get this error. I checked the SPI-SDI net

    but could not see anything wrong. So, What does this error mean ?

    Is it a critical one ?

     

    Best regards,

     

    Firat

    It normally is critical because it means that two outputs are

    connected together. This can mean i.e. that one output provides a

    high supply voltge and the other one the ground. Result will be a

    nice smell of Amps. Only open collector outputs may be connected

    together and perhaps tristate outputs with appropriate control.

    Maybe just the direction of a pin is wrong in a library.

     

    Hi,

     

    Thanks for the reply. I will check it again. But the SPI-SDI net is

    connected to the SDO pins of the SPI devices and SDI pin of the mcu. I

    would rather delete SPI-SDI and create it again.

     

    As Joern suggested, check the direction of the pins in the library where

    each part comes from.  Maybe the SDI pin of the MCU is not defined as an

    input.

     

    --

    Bert Menkveld

     

     

    Hi,

     

    Thanks you to all. As you suggested, the SDO pin of one of the spi

    devices is defined as output. So, there is nothing to correct for this

    issue.

     

    Thanks again,

     

    Regards,

     

    Firat