Hi,
When i run erc command i get this error. I checked the SPI-SDI net but
could not see anything wrong. So, What does this error mean ? Is it a
critical one ?
Best regards,
Firat
Hi,
When i run erc command i get this error. I checked the SPI-SDI net but
could not see anything wrong. So, What does this error mean ? Is it a
critical one ?
Best regards,
Firat
Firat Kocak wrote:
Joern Paschedag wrote:
Firat Kocak schrieb:
Hi,
When i run erc command i get this error. I checked the SPI-SDI net
but could not see anything wrong. So, What does this error mean ?
Is it a critical one ?
Best regards,
Firat
It normally is critical because it means that two outputs are
connected together. This can mean i.e. that one output provides a
high supply voltge and the other one the ground. Result will be a
nice smell of Amps. Only open collector outputs may be connected
together and perhaps tristate outputs with appropriate control.
Maybe just the direction of a pin is wrong in a library.
Hi,
Thanks for the reply. I will check it again. But the SPI-SDI net is
connected to the SDO pins of the SPI devices and SDI pin of the mcu. I
would rather delete SPI-SDI and create it again.
As Joern suggested, check the direction of the pins in the library where
each part comes from. Maybe the SDI pin of the MCU is not defined as an
input.
--
Bert Menkveld
Firat Kocak wrote:
Joern Paschedag wrote:
Firat Kocak schrieb:
Hi,
When i run erc command i get this error. I checked the SPI-SDI net
but could not see anything wrong. So, What does this error mean ?
Is it a critical one ?
Best regards,
Firat
It normally is critical because it means that two outputs are
connected together. This can mean i.e. that one output provides a
high supply voltge and the other one the ground. Result will be a
nice smell of Amps. Only open collector outputs may be connected
together and perhaps tristate outputs with appropriate control.
Maybe just the direction of a pin is wrong in a library.
Hi,
Thanks for the reply. I will check it again. But the SPI-SDI net is
connected to the SDO pins of the SPI devices and SDI pin of the mcu. I
would rather delete SPI-SDI and create it again.
As Joern suggested, check the direction of the pins in the library where
each part comes from. Maybe the SDI pin of the MCU is not defined as an
input.
--
Bert Menkveld