EAGLE User Support (English) How do I remove layers from the display/route list?
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
  • Replies 6 replies
  • Subscribers 178 subscribers
  • Views 327 views
  • Users 0 members are here
Related

How do I remove layers from the display/route list?

autodeskguest
autodeskguest over 17 years ago

I have the Pro version of EAGLE, both v4.16r2 and v5.3.0.  Lately I've

been working on 2 layers boards (layers 1 and 16),  but the display

list of layers always includes layers 2 - 15.  When I manually route a

trace, layers 2 - 15 are also displayed, so I have to ignore the extra

layers in the list.  In DRC/Layers, I have (1*16), so why do I see

these superfluous layers?  EAGLE won't let me delete internal layers,

so what do I do?

 

-Dave Pollum

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    I have the Pro version of EAGLE, both v4.16r2 and v5.3.0.  Lately I've

    been working on 2 layers boards (layers 1 and 16),  but the display

    list of layers always includes layers 2 - 15.  When I manually route a

    trace, layers 2 - 15 are also displayed, so I have to ignore the extra

    layers in the list.  In DRC/Layers, I have (1*16), so why do I see

    these superfluous layers?  EAGLE won't let me delete internal layers,

    so what do I do?

     

    -Dave Pollum

     

    See the Eagle ver 5.x layers help and the example "mylayers.scr" at the very bottom. Set used_layers....

     

    --

    Gruß / regards

     

    Jörn

     

    I have the same 'problem', never seen it as a problem though...

    mylayers.scr does not list 2-15 and the DRC is (1*16)...

     

    Set Used_Layers 1  16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 \

                    31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 \

                    47 48 49 50 51 52   91 92 93 94 95 96;

    DISPLAY NONE 1 16 17 21;

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    I have the Pro version of EAGLE, both v4.16r2 and v5.3.0.  Lately I've

    been working on 2 layers boards (layers 1 and 16),  but the display

    list of layers always includes layers 2 - 15.  When I manually route a

    trace, layers 2 - 15 are also displayed, so I have to ignore the extra

    layers in the list.  In DRC/Layers, I have (1*16), so why do I see

    these superfluous layers?  EAGLE won't let me delete internal layers,

    so what do I do?

     

    -Dave Pollum

     

    See the Eagle ver 5.x layers help and the example "mylayers.scr" at the very bottom. Set used_layers....

     

    --

    Gruß / regards

     

    Jörn

     

    I have the same 'problem', never seen it as a problem though...

    mylayers.scr does not list 2-15 and the DRC is (1*16)...

     

    Set Used_Layers 1  16 17 18 19 20 21 22 23 24 25 26 27 28 29 30 \

                    31 32 33 34 35 36 37 38 39 40 41 42 43 44 45 46 \

                    47 48 49 50 51 52   91 92 93 94 95 96;

    DISPLAY NONE 1 16 17 21;