Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Multiple copies of an element have all pins connected
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 410 views
  • Users 0 members are here
Related

Multiple copies of an element have all pins connected

jrychter
jrychter over 12 years ago

I created a new element in my library. It works fine as long as there is only one copy in the schematic. But if I place another copy (e.g. if I drop two elements into the schematic) my PCB shows all pins of the first and second element connected, as if they had the same names. So far they aren't connected to anything in the schematic.

 

Obviously I did something wrong while creating the library part — but what?

  • Sign in to reply
  • Cancel
  • jrychter
    0 jrychter over 12 years ago in reply to autodeskguest

    Thanks! Now I looked closer and indeed, not *all* the pins are connected, just the ones that are "pwr". This chip has lots of "pwr" pins.

     

    So from what I understand this essentially isn't a problem, because once I wire the schematic everything will be OK.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago

    Jan Rychter wrote:

     

    I created a new element in my library. It works fine as long as there is

    only one copy in the schematic. But if I place another copy (e.g. if I

    drop two elements into the schematic) my PCB shows all pins of the first

    and second element connected, as if they had the same names. So far they

    aren't connected to anything in the schematic.

     

    Obviously I did something wrong while creating the library part — but

    what?

     

    check the direction setting of the pins in the symbol.

     

    All pins with direction set to 'pwr' or 'sup' with the same name are

    connected automatically.

     

    You can override this connection though, by connecting a net to the

    pin in the schematic.

     

    See 'help pin'.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer