EAGLE User Support (English) Question on SMT part packaging?
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 331 views
  • Users 0 members are here
Related

Question on SMT part packaging?

Former Member
Former Member over 12 years ago

Hi,

 

I've made a little board in Eagle using parts from the SFE and Adafruit libraries and I'm ordering parts from Digikey. I wan't to make sure I'm ordering the right parts.

 

On the BOM I have part C1:

 

Part Value         Device                Package           Description
C1   10uF          CAP_POL1206           EIA3216           Capacitor Polarized

 

 

and another 10uF capacitor:

Part Value         Device                Package           Description
C6   10uF          CAP1206               1206              Capacitor  

 

 

Under "Device" both of the caps are 1206, but for package C6 is 1206 and C1 is EIA3216, which from my understanding means they're both the same, where 1206 is imperial and 3216 is metric. So could I buy this capacitor (http://www.digikey.com/product-detail/e ... ND/2103160) and use it for both C1 and C6?

 

Thanks for the help!

  • Sign in to reply
  • Cancel
Parents
  • fritzz
    0 fritzz over 12 years ago

    c1 says "polarized". That cap on Digikey is non polarized.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • fritzz
    0 fritzz over 12 years ago

    c1 says "polarized". That cap on Digikey is non polarized.