Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Device pin connections on schemitic
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 1212 views
  • Users 0 members are here
Related

Device pin connections on schemitic

e14 Contributor
e14 Contributor over 12 years ago

I have been looking for a tutorial or detailed explanation
of how to produce custom device profiles in the eagle library.  There is something I am missing; I cannot seam
to get my attempts to make a simple device work as expected.

 

I am designing a board that will have a number of Molex KK
3.96 mm pin connectors on it. Since I was unsuccessful at locating any existing
library devices with a  3.96 mm pin pitch
I thought I could produce my own device profile by modifying an existing library
file.  I started with the MA04-1 pin header
profile in he con_lstb.lbr. This is essentially the same connector device
profile as I need with a pin pitch of 2.54 mm instead of the 3.96 m that I will
require.  My approach was to modify the  MA04-1 package so that the pads are centered
on a 3.96mm grid and save it as a different package variant. I then verified that
the pins are connected to the pads in the connect window for the device. 

 

As a result of my efforts to make a new variant package neither
the original device nor my newly created variant are working as expected. I can
select this device and place it on a schematic as expected. The device symbol appears
on the schematic and package image appears on the board as expected. The problem
is I cannot seam to make any valid connections to the device on the schematic.
Any connection I attempt to make never appear on the board ratsnest , I get  ECR errors indicating no connection have bean
made to the device. No matter what I do I cannot make a connection to the pins
on the device.

 

 

 

 

 

What am I doing wrong?

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 15/11/13 18:36, Darryl Dennis wrote:

    I am designing a board that will have a number of Molex KK

    3.96 mm pin connectors on it. Since I was unsuccessful at locating any

    existing

    library devices with a  3.96 mm pin pitch

     

    I've designed in a KK 3.96 on one board, so I must have found or (more

    likely) created such a library. If the latter I would have thought I'd

    have uploaded it to the CadSoft site. However, I don't see it there, so...

     

    As I thought. Check the "con-molex" library in the standard

    distribution. It has a range of KK-156 parts. 0.156" is 3.96mm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 15/11/13 18:36, Darryl Dennis wrote:

    I am designing a board that will have a number of Molex KK

    3.96 mm pin connectors on it. Since I was unsuccessful at locating any

    existing

    library devices with a  3.96 mm pin pitch

     

    I've designed in a KK 3.96 on one board, so I must have found or (more

    likely) created such a library. If the latter I would have thought I'd

    have uploaded it to the CadSoft site. However, I don't see it there, so...

     

    As I thought. Check the "con-molex" library in the standard

    distribution. It has a range of KK-156 parts. 0.156" is 3.96mm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to autodeskguest

    Thanks! that is what I was trying to find. I am still very
    interested in what I did wrong; how I could successfully make my own device profile?
    It seams that it should be straight forward.
    I would like to have a better understanding of the library files and how they
    are made.