EAGLE User Support (English) exporting schematics to pictures
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
  • Replies 6 replies
  • Subscribers 179 subscribers
  • Views 1054 views
  • Users 0 members are here
Related

exporting schematics to pictures

autodeskguest
autodeskguest over 17 years ago

On this site:

 

http://www.societyofrobots.com/member_tutorials/node/91

 

is an Eagle Schematic. It is interesting because the line widths are

bigger than anything I have managed to obtain with Eagle 4.9.x The

proportions are much better than I get. Anyone got good advice on how to

do exporting to pictures for both print and the web that produces good

results?

 

I can make the net line thicker but can't seem to make the default width

change and even then I can't see how to change the width of the lines in

the IO pins.

 

Thanks

 

Pete

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Gary Gofstein wrote:

    Many of the EAGLE exports generate some kind of bitmapped file, you must

    set the resolution in dots per inch. The default value (75?) is rather

    low, but bitmapped images are often large in bytes and do not always

    scale well...so

     

    I like to use the sch2wmf ULP to generate native windows drawings which

    scale perfectly and are compact. These can be pasted into documents and

    saved as pdf's and are totally zoomable and scalable.

    Thank you for that suggestion. And Joern for his. I didn't know about

    the WMF ULP.

     

    However, nice though they are, neither can get the results I saw with a

    much better proportioning to the line widths.

     

    Pete

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Gary Gofstein wrote:

    Many of the EAGLE exports generate some kind of bitmapped file, you must

    set the resolution in dots per inch. The default value (75?) is rather

    low, but bitmapped images are often large in bytes and do not always

    scale well...so

     

    I like to use the sch2wmf ULP to generate native windows drawings which

    scale perfectly and are compact. These can be pasted into documents and

    saved as pdf's and are totally zoomable and scalable.

    Thank you for that suggestion. And Joern for his. I didn't know about

    the WMF ULP.

     

    However, nice though they are, neither can get the results I saw with a

    much better proportioning to the line widths.

     

    Pete