EAGLE User Support (English) exporting schematics to pictures
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
  • Replies 6 replies
  • Subscribers 179 subscribers
  • Views 1051 views
  • Users 0 members are here
Related

exporting schematics to pictures

autodeskguest
autodeskguest over 17 years ago

On this site:

 

http://www.societyofrobots.com/member_tutorials/node/91

 

is an Eagle Schematic. It is interesting because the line widths are

bigger than anything I have managed to obtain with Eagle 4.9.x The

proportions are much better than I get. Anyone got good advice on how to

do exporting to pictures for both print and the web that produces good

results?

 

I can make the net line thicker but can't seem to make the default width

change and even then I can't see how to change the width of the lines in

the IO pins.

 

Thanks

 

Pete

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Hej Peter,

     

    You can use the export function as image, and then with a litle tweaking you

    get a nice result.

    And you can always use the print screen function of you computer, i think

    that's what he used.

     

    Succes

     

    "peter harrison" <peteh@cannock.ac.uk> schreef in bericht

    news:ghbevr$rph$1@cheetah.cadsoft.de...

    On this site:

     

    http://www.societyofrobots.com/member_tutorials/node/91

     

    is an Eagle Schematic. It is interesting because the line widths are

    bigger than anything I have managed to obtain with Eagle 4.9.x The

    proportions are much better than I get. Anyone got good advice on how to

    do exporting to pictures for both print and the web that produces good

    results?

     

    I can make the net line thicker but can't seem to make the default width

    change and even then I can't see how to change the width of the lines in

    the IO pins.

     

    Thanks

     

    Pete

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    peter harrison schrieb:

    On this site:

     

    http://www.societyofrobots.com/member_tutorials/node/91

     

    is an Eagle Schematic. It is interesting because the line widths are

    bigger than anything I have managed to obtain with Eagle 4.9.x The

    proportions are much better than I get. Anyone got good advice on how to

    do exporting to pictures for both print and the web that produces good

    results?

     

    I can make the net line thicker but can't seem to make the default width

    change and even then I can't see how to change the width of the lines in

    the IO pins.

     

    Thanks

     

    Pete

     

    Just use the exp2image.ulp image if you just run it you get a little

    window. Use the help part of it to get an example. Or in the schematic

    just enter at the command line:

    run exp2image color 150 .png 91 92 94 95 96;

    This will run the ulp with color output as .png file with layers 91 to

    96 except layer 93.

     

    --

    Gruß / regards

     

    Jörn

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Many of the EAGLE exports generate some kind of bitmapped file, you must

    set the resolution in dots per inch. The default value (75?) is rather

    low, but bitmapped images are often large in bytes and do not always

    scale well...so

     

    I like to use the sch2wmf ULP to generate native windows drawings which

    scale perfectly and are compact. These can be pasted into documents and

    saved as pdf's and are totally zoomable and scalable.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Gary Gofstein wrote:

    Many of the EAGLE exports generate some kind of bitmapped file, you must

    set the resolution in dots per inch. The default value (75?) is rather

    low, but bitmapped images are often large in bytes and do not always

    scale well...so

     

    I like to use the sch2wmf ULP to generate native windows drawings which

    scale perfectly and are compact. These can be pasted into documents and

    saved as pdf's and are totally zoomable and scalable.

    Thank you for that suggestion. And Joern for his. I didn't know about

    the WMF ULP.

     

    However, nice though they are, neither can get the results I saw with a

    much better proportioning to the line widths.

     

    Pete

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 17 years ago

    Peter Harrison schrieb:

    Gary Gofstein wrote:

    Many of the EAGLE exports generate some kind of bitmapped file, you

    must set the resolution in dots per inch. The default value (75?) is

    rather low, but bitmapped images are often large in bytes and do not

    always scale well...so

     

    I like to use the sch2wmf ULP to generate native windows drawings

    which scale perfectly and are compact. These can be pasted into

    documents and saved as pdf's and are totally zoomable and scalable.

    Thank you for that suggestion. And Joern for his. I didn't know about

    the WMF ULP.

     

    However, nice though they are, neither can get the results I saw with a

    much better proportioning to the line widths.

     

    Pete

     

     

    The default line width for nets is 6 mil. This fits to the line

    width of the pins. You can change the default value for the net

    lines with, for example:

     

    SET NET_WIRE_WIDTH 0.01;

     

    The pin width can't be changed.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago in reply to Richard_H

    Richard Hammerl wrote:

    Peter Harrison schrieb:

    Gary Gofstein wrote:

    Many of the EAGLE exports generate some kind of bitmapped file, you

    must set the resolution in dots per inch. The default value (75?) is

    rather low, but bitmapped images are often large in bytes and do not

    always scale well...so

     

    I like to use the sch2wmf ULP to generate native windows drawings

    which scale perfectly and are compact. These can be pasted into

    documents and saved as pdf's and are totally zoomable and scalable.

    Thank you for that suggestion. And Joern for his. I didn't know about

    the WMF ULP.

     

    However, nice though they are, neither can get the results I saw with a

    much better proportioning to the line widths.

     

    Pete

     

    The default line width for nets is 6 mil. This fits to the line

    width of the pins. You can change the default value for the net

    lines with, for example:

     

    SET NET_WIRE_WIDTH 0.01;

     

    The pin width can't be changed.

     

    Ah ... right. Thanks for that. Clearly then, the picture I saw has been

    post-processed. I did manage a similar effect by exporting to WMF and

    then messing in Illustrator but it all seemed a lot of work for the result.

     

    Pete