EAGLE User Support (English) exporting schematics to pictures
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
  • Replies 6 replies
  • Subscribers 179 subscribers
  • Views 1057 views
  • Users 0 members are here
Related

exporting schematics to pictures

autodeskguest
autodeskguest over 17 years ago

On this site:

 

http://www.societyofrobots.com/member_tutorials/node/91

 

is an Eagle Schematic. It is interesting because the line widths are

bigger than anything I have managed to obtain with Eagle 4.9.x The

proportions are much better than I get. Anyone got good advice on how to

do exporting to pictures for both print and the web that produces good

results?

 

I can make the net line thicker but can't seem to make the default width

change and even then I can't see how to change the width of the lines in

the IO pins.

 

Thanks

 

Pete

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 17 years ago

    Peter Harrison schrieb:

    Gary Gofstein wrote:

    Many of the EAGLE exports generate some kind of bitmapped file, you

    must set the resolution in dots per inch. The default value (75?) is

    rather low, but bitmapped images are often large in bytes and do not

    always scale well...so

     

    I like to use the sch2wmf ULP to generate native windows drawings

    which scale perfectly and are compact. These can be pasted into

    documents and saved as pdf's and are totally zoomable and scalable.

    Thank you for that suggestion. And Joern for his. I didn't know about

    the WMF ULP.

     

    However, nice though they are, neither can get the results I saw with a

    much better proportioning to the line widths.

     

    Pete

     

     

    The default line width for nets is 6 mil. This fits to the line

    width of the pins. You can change the default value for the net

    lines with, for example:

     

    SET NET_WIRE_WIDTH 0.01;

     

    The pin width can't be changed.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 17 years ago

    Peter Harrison schrieb:

    Gary Gofstein wrote:

    Many of the EAGLE exports generate some kind of bitmapped file, you

    must set the resolution in dots per inch. The default value (75?) is

    rather low, but bitmapped images are often large in bytes and do not

    always scale well...so

     

    I like to use the sch2wmf ULP to generate native windows drawings

    which scale perfectly and are compact. These can be pasted into

    documents and saved as pdf's and are totally zoomable and scalable.

    Thank you for that suggestion. And Joern for his. I didn't know about

    the WMF ULP.

     

    However, nice though they are, neither can get the results I saw with a

    much better proportioning to the line widths.

     

    Pete

     

     

    The default line width for nets is 6 mil. This fits to the line

    width of the pins. You can change the default value for the net

    lines with, for example:

     

    SET NET_WIRE_WIDTH 0.01;

     

    The pin width can't be changed.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 17 years ago in reply to Richard_H

    Richard Hammerl wrote:

    Peter Harrison schrieb:

    Gary Gofstein wrote:

    Many of the EAGLE exports generate some kind of bitmapped file, you

    must set the resolution in dots per inch. The default value (75?) is

    rather low, but bitmapped images are often large in bytes and do not

    always scale well...so

     

    I like to use the sch2wmf ULP to generate native windows drawings

    which scale perfectly and are compact. These can be pasted into

    documents and saved as pdf's and are totally zoomable and scalable.

    Thank you for that suggestion. And Joern for his. I didn't know about

    the WMF ULP.

     

    However, nice though they are, neither can get the results I saw with a

    much better proportioning to the line widths.

     

    Pete

     

    The default line width for nets is 6 mil. This fits to the line

    width of the pins. You can change the default value for the net

    lines with, for example:

     

    SET NET_WIRE_WIDTH 0.01;

     

    The pin width can't be changed.

     

    Ah ... right. Thanks for that. Clearly then, the picture I saw has been

    post-processed. I did manage a similar effect by exporting to WMF and

    then messing in Illustrator but it all seemed a lot of work for the result.

     

    Pete