EAGLE User Support (English) Adding LMC7101 Op Amp To Schematic
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 177 subscribers
  • Views 1020 views
  • Users 0 members are here
Related

Adding LMC7101 Op Amp To Schematic

Former Member
Former Member over 12 years ago

Hi guys,

 

This is my first ever post on these forums and i've only been registered for 10 minutes so i apologize in advance for any nooby question i may ask. I'm fairly new with the EAGLE software as i've only seen some tutorials and played around a little bit with its functionalities. I'm yet to do anything more serious but that's what I intend to do in time.

 

So my question. I'm trying to design a schematic of a circuit I have already implemented on a breadboard but I can't seem to find one of the components I need in the libraries, a LMC7101 op amp. I've done a quick search here in the forums but I've come up short although I could have missed something. I also did a google search but again I came up short. So what I want to ask is: is there anyway to include this component in my EAGLE software (version 5.3.0 btw) so I can use it? Like adding extra libraries?

 

My final goal is to design a PCB with several of these op amps so I really to include it in my schematics.

 

Regards,

 

Miguel

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 16/12/13 19:03, Miguel Almeida wrote:

    I can't seem to find one of the

    components I need in the libraries, a LMC7101 op amp.

     

    Depending on the details of that part, it may well be sufficient to use

    one of the generic op-amps in the linear library. However...

     

     

    So what I want to ask is: is there anyway to include this component in

    my EAGLE software (version 5.3.0 btw) so I can use it? Like adding extra

    libraries?

     

    Of course. It wouldn't be much use if you couldn't.

     

    Surely you must have come across a tutorial (such as the one in the

    Eagle documentation supplied with the software) on creating library

    parts? For your purposes you probably want to start by copying an

    existing op-amp (e.g. from linear.lbr) into your new library, then copy

    in the required package from ref-packages.lbr if necessary. You may need

    to tweak the symbol a bit, but probably all you need then is to make a

    device (add symbol and package, set pin-outs).

     

    This is actually a nice easy introduction to an important part of using

    Eagle (or any PCB CAD tool, actually).

     

    HTH,

    Rob

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 12 years ago

    On 16/12/13 19:03, Miguel Almeida wrote:

    I can't seem to find one of the

    components I need in the libraries, a LMC7101 op amp.

     

    Depending on the details of that part, it may well be sufficient to use

    one of the generic op-amps in the linear library. However...

     

     

    So what I want to ask is: is there anyway to include this component in

    my EAGLE software (version 5.3.0 btw) so I can use it? Like adding extra

    libraries?

     

    Of course. It wouldn't be much use if you couldn't.

     

    Surely you must have come across a tutorial (such as the one in the

    Eagle documentation supplied with the software) on creating library

    parts? For your purposes you probably want to start by copying an

    existing op-amp (e.g. from linear.lbr) into your new library, then copy

    in the required package from ref-packages.lbr if necessary. You may need

    to tweak the symbol a bit, but probably all you need then is to make a

    device (add symbol and package, set pin-outs).

     

    This is actually a nice easy introduction to an important part of using

    Eagle (or any PCB CAD tool, actually).

     

    HTH,

    Rob