EAGLE User Support (English) How do I redefine the PCB (board area)?
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
  • State Not Answered
  • Replies 4 replies
  • Subscribers 179 subscribers
  • Views 821 views
  • Users 0 members are here
  • eagle
  • layout
  • pcb
  • board_area
Related

How do I redefine the PCB (board area)?

Former Member
Former Member over 12 years ago

Hi,

 

I started learning Eagle by putting existing boards into the schematic editor and then attempting to do the layout the same as the existing board.  The problem I have that not all boards are square or rectangular.  How can i redefine the board area to match the project I am working on.  For example, the one robot kit I build has a circular board with three "tentacles" protruding to the front where IR led's are mounted.  It also has a add on board which solders onto the main board.  How do add that extra little board into the equation?

 

Thank you

WeideJUR

  • Sign in to reply
  • Cancel
Parents
  • tonnie_wittenaar
    0 tonnie_wittenaar over 12 years ago

    What you can do with odd shapes is to design the outline in an DXF editor.

     

    Look at http://www.ilovefreesoftware.com/10/featured/5-free-autocad-editors-to-edit-dwg-dxf-file-formats.html for 5 free dxf editors to select from.

     

    Once you created the DXF file, you can simple import this in eagle board layout using a User Language Program: dxfimport.ulp

    Latest version you can find here: http://www.cadsoftusa.com/downloads/file/dxfimport1_3.zip

    Just folow the instructions in the ULP and there is your outline.

     

    Wish you succes with this!

     

    Regards

    Tonnie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to tonnie_wittenaar

    The importing of the DFX file worked B-E-A-Utifully!  Thank you thewillows

     

    All I need to do now is to upgrade from the lite version so I can place the components where they should go on the board since it stretches outside the (100 80) limit of the light version.

     

    Regards,

    Jurie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tonnie_wittenaar
    0 tonnie_wittenaar over 11 years ago in reply to Former Member

    Hi Jurie,

     

    Nice when a plan comes together!

    Many luck with it

     

    Regards

    Tonnie

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tonnie_wittenaar
    0 tonnie_wittenaar over 11 years ago in reply to Former Member

    Hi Jurie,

     

    Nice when a plan comes together!

    Many luck with it

     

    Regards

    Tonnie