EAGLE User Support (English) VIA Drill size
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
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 230 views
  • Users 0 members are here
Related

VIA Drill size

autodeskguest
autodeskguest over 17 years ago

How do I define the 'standard' via drill size.  I have 24mils set in the DRC

file and the autorouter creates the correct size VIA's.  BUT when I either

manually place a VIA or transition between layers while manually routing the

VIA drill size is set to 23.622.  This drill size then fails the DRC check

until I resize it to 24, or if I remeber to change the size when manually

using VIA's.  I am sure there is an easy way, I am just able to find it in

the documentation/help files.

 

Phil

 

 

 

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 17 years ago

    PhilK schrieb:

    How do I define the 'standard' via drill size.  I have 24mils set in the DRC

    file and the autorouter creates the correct size VIA's.  BUT when I either

    manually place a VIA or transition between layers while manually routing the

    VIA drill size is set to 23.622.  This drill size then fails the DRC check

    until I resize it to 24, or if I remeber to change the size when manually

    using VIA's.  I am sure there is an easy way, I am just able to find it in

    the documentation/help files.

     

    Phil

     

     

     

     

    This can be set in eagle.scr in the BRD: section.

     

    CHANGE DRILL 24mil ;

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm