EAGLE User Support (English) How can I create an Edge pin PCB to mate to a Foxconn Connector?
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
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 182 subscribers
  • Views 1892 views
  • Users 0 members are here
  • board
  • eagle
  • pins
  • pcb
  • edge
  • question
Related

How can I create an Edge pin PCB to mate to a Foxconn Connector?

japper
japper over 12 years ago

I have a project where I need to design a PCB with the edge pins that are
compatible with a Foxconn AS0B326-S55N-7F or Foxconn AS0B326-S78N-7F connector.

 

Are there any libraries for the Foxconn parts menitoned above and how are edge pins created in the
Eaglecad schematic/layout tools?

 

Are the PCB edge pins typically also a library type part like the mating connector?

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    0 dukepro over 12 years ago

    On 01/15/2014 09:28 AM, japper wrote:

    I have a project where I need to design a PCB with the edge pins that

    are

    compatible with a Foxconn AS0B326-S55N-7F or Foxconn AS0B326-S78N-7F

    connector.

     

    Are there any libraries for the Foxconn parts menitoned above and how

    are edge pins created in the

    Eaglecad schematic/layout tools?

     

    Japper,

     

    I can't help you with the specific Foxconn connector, but I can help

    with creating edge connectors in Eagle.

     

    Look for my post on 21-Jan-2014 titled "Re: Help for footprint (edge

    mounted connector)".  I posted card-edge.lbr.zip which contains a 50-pin

    edge connector setup in three different packages - one for the left end

    of the edge, one for the right end of the edge, and one for somewhere in

    between.

     

    I believe a link to the thread is

    http://www.element14.com/community/message/101512.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dukepro
    0 dukepro over 12 years ago

    On 01/15/2014 09:28 AM, japper wrote:

    I have a project where I need to design a PCB with the edge pins that

    are

    compatible with a Foxconn AS0B326-S55N-7F or Foxconn AS0B326-S78N-7F

    connector.

     

    Are there any libraries for the Foxconn parts menitoned above and how

    are edge pins created in the

    Eaglecad schematic/layout tools?

     

    Japper,

     

    I can't help you with the specific Foxconn connector, but I can help

    with creating edge connectors in Eagle.

     

    Look for my post on 21-Jan-2014 titled "Re: Help for footprint (edge

    mounted connector)".  I posted card-edge.lbr.zip which contains a 50-pin

    edge connector setup in three different packages - one for the left end

    of the edge, one for the right end of the edge, and one for somewhere in

    between.

     

    I believe a link to the thread is

    http://www.element14.com/community/message/101512.

     

    HTH,

        - Chuck