EAGLE User Support (English) How can I create an Edge pin PCB to mate to a Foxconn Connector?
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
  • State Verified Answer
  • Replies 10 replies
  • Subscribers 182 subscribers
  • Views 1915 views
  • Users 0 members are here
  • board
  • eagle
  • pins
  • pcb
  • edge
  • question
Related

How can I create an Edge pin PCB to mate to a Foxconn Connector?

japper
japper over 12 years ago

I have a project where I need to design a PCB with the edge pins that are
compatible with a Foxconn AS0B326-S55N-7F or Foxconn AS0B326-S78N-7F connector.

 

Are there any libraries for the Foxconn parts menitoned above and how are edge pins created in the
Eaglecad schematic/layout tools?

 

Are the PCB edge pins typically also a library type part like the mating connector?

 

Thanks

  • Sign in to reply
  • Cancel
  • japper
    0 japper over 12 years ago

    Anyone have an answer for this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to japper

    Have a look in con-pc.lbr

     

    The will give you a good idea how to create a PCB edge connector

     

    All the best

    Warren

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • japper
    0 japper over 12 years ago in reply to autodeskguest

    Thanks Warren-

     

    I actually found a QSeven library on this site late yesterday that has the whole board outline

    so I am a happy camper now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to japper

    Can you please share the link to that QSeven library, i am having a hard time finding it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • japper
    0 japper over 12 years ago in reply to Former Member

    The Q7 library on the EagleCad library site only had a library part that allowed for the mating connector and outline

    of the Q7 board to be added to a carrier type PCB.

     

    I took that and modified it into a library part within its own library for the actual Q7 pcb with edge fingers.

     

    I will consider uploading it after I receive my PCB next week and have an opportunity to verify that it is good to go as I am new

    to making library parts and not sure how to add this part to an exisiting library...


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to japper

    Can you provide a link to Q7 library on eaglecad library site?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 12 years ago

    On 01/15/2014 09:28 AM, japper wrote:

    I have a project where I need to design a PCB with the edge pins that

    are

    compatible with a Foxconn AS0B326-S55N-7F or Foxconn AS0B326-S78N-7F

    connector.

     

    Are there any libraries for the Foxconn parts menitoned above and how

    are edge pins created in the

    Eaglecad schematic/layout tools?

     

    Japper,

     

    I can't help you with the specific Foxconn connector, but I can help

    with creating edge connectors in Eagle.

     

    Look for my post on 21-Jan-2014 titled "Re: Help for footprint (edge

    mounted connector)".  I posted card-edge.lbr.zip which contains a 50-pin

    edge connector setup in three different packages - one for the left end

    of the edge, one for the right end of the edge, and one for somewhere in

    between.

     

    I believe a link to the thread is

    http://www.element14.com/community/message/101512.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 12 years ago in reply to Former Member

    On 22/02/2014 14:04, rajat goyal wrote:

    Can you provide a link to Q7 library on eaglecad library site?

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/104532

     

    http://www.cadsoft.de/downloads/libraries

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 12 years ago in reply to autodeskguest

    Thanks, Mate.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • japper
    0 japper over 12 years ago in reply to Former Member

    rajat goyal wrote:

     

    Can you provide a link to Q7 library on eaglecad library site?

    The two that I found were for the mating connector at the following links:

     

    http://www.cadsoftusa.com/downloads/file/qseven.lbr

     

    http://www.cadsoftusa.com/downloads/file/qseven-yamaichi.lbr

     

    These libraries are not mine, I just found them on that site, so I am not sure if they are good or not but I 'copied the Qseven.lbr

    and then used  the pin spacing and board outline and changed that part to be the actualQ7 module and not the mating connector

    for a carrier board as this qseven.lib library (in the link above) contains.