EAGLE User Support (English) Help for footprint (edge mounted connector)
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
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 183 subscribers
  • Views 1500 views
  • Users 0 members are here
Related

Help for footprint (edge mounted connector)

cgroen
cgroen over 12 years ago

Hello,

I'm doing my first few boards in Eagle, and so far everything is running perfectly (and will upgrade to the full version now) image

On a new board I'm trying to do I have two 6 pin connectors that I would like to mount on the edge of the board (horisontal). I'm having a hard time how to design that as a footprint. There needs to be to cutouts in the board and these should be plated. I have attached a picture of the connecotor and a picture of how it has been done in another product.

Any help out there ? This is the last thing I need to resolve before my board is being sent (I'm using PCB-POOL)

 

Thanks for any help (would even consider paying you for a ready made footprint that would do this if reasonable..)

 

 

image

image

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    0 dukepro over 12 years ago

    Carsten,

     

    The attached isn't exactly what you want, but it should serve as a guide

    on how to design an edge connector.  It's a 50-pin card edge connector

    with three different configurations - left end of board edge, right end

    of board edge, and middle of board edge.  As Richard mentioned, you will

    have to work with your board house to specify the gold plating.

     

    Note that zero-width wires are placed in the Dimension layer to specify

    the cutout.  What's NOT in the design is a polygon or rectangle that

    specifies the top and bottom finish.  Eagle has tFinish and bFinish

    layers to specify exactly this.  You can add sections to your CAM job to

    produce gerber files for these two layers, then name the output files

    AuTop.gbr and AuBot.gbr.  That and a note in the README file should make

    it pretty obvious to the board house which pads should be gold plated.

     

    Argh!!!  I had to zip the file to get it to post - it's just a hair over

    50k unzipped.

     

    HTH,

        - Chuck

     

     

    On 01/20/2014 11:00 AM, Carsten Groen wrote:

    Hello,

    I'm doing my first few boards in Eagle, and so far everything is running

    perfectly (and will upgrade to the full version now) image

    On a new board I'm trying to do I have two 6 pin connectors that I would

    like to mount on the edge of the board (horisontal). I'm having a hard

    time how to design that as a footprint. There needs to be to cutouts in

    the board and these should be plated. I have attached a picture of the

    connecotor and a picture of how it has been done in another product.

    Any help out there ? This is the last thing I need to resolve before my

    board is being sent (I'm using PCB-POOL)

     

    Thanks for any help (would even consider paying you for a ready made

    footprint that would do this if reasonable..)

     

     

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/101512

     

     

    Attachments:
    card-edge.lbr.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to dukepro

    Chuck -

     

    Very helpful library!

     

    I am modifying your CARDEDGE-50 to be a 72-pin edge connector that I need.

     

    I noticed that the odd-numbered SMD's in CARDEDGE-50 did not exclude stop and cream. That is, the did not have the stop="no" cream="no" attribute. See below.

     

    All the other SMDs in the library did.

     

    Is this by design, and, if so, for what reason?

     

    <smd name="4" x="-27.94" y="5.08" dx="1.397" dy="10.16" layer="1" stop="no" cream="no"/>

    <smd name="2" x="-30.48" y="5.08" dx="1.397" dy="10.16" layer="1" stop="no" cream="no"/>

    <smd name="21" x="-5.08" y="5.08" dx="1.397" dy="10.16" layer="16" rot="R180"/>

    <smd name="23" x="-2.54" y="5.08" dx="1.397" dy="10.16" layer="16" rot="R180"/>

     

    I am making a simple extender card so I'm not sure it matters. But I certainly would like to know.

     

    Thanks again for the great card-edge library!

     

    Cameron Jones

    Synclavier Digital

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to dukepro

    Chuck -

     

    Very helpful library!

     

    I am modifying your CARDEDGE-50 to be a 72-pin edge connector that I need.

     

    I noticed that the odd-numbered SMD's in CARDEDGE-50 did not exclude stop and cream. That is, the did not have the stop="no" cream="no" attribute. See below.

     

    All the other SMDs in the library did.

     

    Is this by design, and, if so, for what reason?

     

    <smd name="4" x="-27.94" y="5.08" dx="1.397" dy="10.16" layer="1" stop="no" cream="no"/>

    <smd name="2" x="-30.48" y="5.08" dx="1.397" dy="10.16" layer="1" stop="no" cream="no"/>

    <smd name="21" x="-5.08" y="5.08" dx="1.397" dy="10.16" layer="16" rot="R180"/>

    <smd name="23" x="-2.54" y="5.08" dx="1.397" dy="10.16" layer="16" rot="R180"/>

     

    I am making a simple extender card so I'm not sure it matters. But I certainly would like to know.

     

    Thanks again for the great card-edge library!

     

    Cameron Jones

    Synclavier Digital