EAGLE User Support (English) Issues with 6.5 and MacOS Mavericks
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
  • State Not Answered
  • Replies 24 replies
  • Subscribers 181 subscribers
  • Views 1953 views
  • Users 0 members are here
Related

Issues with 6.5 and MacOS Mavericks

Former Member
Former Member over 11 years ago

Are there configuration work arounds for the following issues ? Configuration is the 6.5.0 version under MacOS 10.9.1

 

1. The directories in Options/directories appear to be ignored and open always dumps me in the Documents folder. It is possible that Mavericks screws up environment variables, so I tried a fully specified path with no luck. Is there an official way to make this work again ?

 

2. When adding components the mouse stops dragging the component after the add command is selected. This can be worked around by moving the window slightly and then the component tracks on the schematic or layout field correctly. This is new behavior with Mavericks, so it is likely that Apple in their wonderful competence changed something. Does a work around exist yet ?

 

Both of these are not show stoppers, but they do get annoying after awhile and probably should be looked at by whomever is doing Cadsoft's Mac support

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest +1
    James Morrison wrote on Sat, 19 April 2014 21:54 Jorge Garcia wrote on Mon, 17 February 2014 11:52 Hi Everyone, If anyone can reproduce or has run into the issues Matt is seeing please reply. I need to…
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 2014-02-07 18:07:44 +0000, Matt Compton <noreply-135375@element14.com> said:

     

    I have seen odd mouse behavior as well. Component can't be dragged,

    lines don't draw with mouse movement, etc. To fix it I do a "Redraw"

    and that brings it back to normal operation. Also seems to be a really

    long delay after some operations before the mouse will respond.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 2014-02-07 18:07:44 +0000, Matt Compton <noreply-135375@element14.com> said:

     

    I have seen odd mouse behavior as well. Component can't be dragged,

    lines don't draw with mouse movement, etc. To fix it I do a "Redraw"

    and that brings it back to normal operation. Also seems to be a really

    long delay after some operations before the mouse will respond.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to autodeskguest

    On 2014-03-28 19:24:48 +0000, Joe <jtowich@montanasky.net> said:

     

    On 2014-02-07 18:07:44 +0000, Matt Compton <noreply-135375@element14.com> said:

     

    I have seen odd mouse behavior as well. Component can't be dragged,

    lines don't draw with mouse movement, etc. To fix it I do a "Redraw"

    and that brings it back to normal operation. Also seems to be a really

    long delay after some operations before the mouse will respond.

     

    I saw more bad behavior with the last layout. Eagle crashed 3 times

    during the layout. This is a little vague, but it seemed to crash if

    you do something that takes time, like select a group and operate on it

    (move, delete, etc). If you move the mouse and click on something

    before it is complete (this is obviously done quickly, but sometimes

    eagle can take a second or two to complete an operation) it sometimes

    crashes. After I made sure operations were complete before moving the

    mouse there were no more crashes. I have an i7 mac book pro with 8 megs

    of RAM running mavericks.