EAGLE User Support (English) Issues with 6.5 and MacOS Mavericks
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
  • State Not Answered
  • Replies 24 replies
  • Subscribers 181 subscribers
  • Views 1951 views
  • Users 0 members are here
Related

Issues with 6.5 and MacOS Mavericks

Former Member
Former Member over 11 years ago

Are there configuration work arounds for the following issues ? Configuration is the 6.5.0 version under MacOS 10.9.1

 

1. The directories in Options/directories appear to be ignored and open always dumps me in the Documents folder. It is possible that Mavericks screws up environment variables, so I tried a fully specified path with no luck. Is there an official way to make this work again ?

 

2. When adding components the mouse stops dragging the component after the add command is selected. This can be worked around by moving the window slightly and then the component tracks on the schematic or layout field correctly. This is new behavior with Mavericks, so it is likely that Apple in their wonderful competence changed something. Does a work around exist yet ?

 

Both of these are not show stoppers, but they do get annoying after awhile and probably should be looked at by whomever is doing Cadsoft's Mac support

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest +1
    James Morrison wrote on Sat, 19 April 2014 21:54 Jorge Garcia wrote on Mon, 17 February 2014 11:52 Hi Everyone, If anyone can reproduce or has run into the issues Matt is seeing please reply. I need to…
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    I seem to be having issue #2 (components not following the cursor around;

    nets not being drawn with cursor movement) as well, although not always.

    Although I only installed EAGLE 6.5.0 yesterday, so I haven't had a lot of

    time to play around with it, it seems like when EAGLE starts in the

    schematic I want to edit, the problem doesn't occur, but when I edit a

    library or something like that and then reopen my schematic, the problem

    occurs.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    I seem to be having issue #2 (components not following the cursor around;

    nets not being drawn with cursor movement) as well, although not always.

    Although I only installed EAGLE 6.5.0 yesterday, so I haven't had a lot of

    time to play around with it, it seems like when EAGLE starts in the

    schematic I want to edit, the problem doesn't occur, but when I edit a

    library or something like that and then reopen my schematic, the problem

    occurs.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.