EAGLE User Support (English) Issues with 6.5 and MacOS Mavericks
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
  • State Not Answered
  • Replies 24 replies
  • Subscribers 181 subscribers
  • Views 1951 views
  • Users 0 members are here
Related

Issues with 6.5 and MacOS Mavericks

Former Member
Former Member over 11 years ago

Are there configuration work arounds for the following issues ? Configuration is the 6.5.0 version under MacOS 10.9.1

 

1. The directories in Options/directories appear to be ignored and open always dumps me in the Documents folder. It is possible that Mavericks screws up environment variables, so I tried a fully specified path with no luck. Is there an official way to make this work again ?

 

2. When adding components the mouse stops dragging the component after the add command is selected. This can be worked around by moving the window slightly and then the component tracks on the schematic or layout field correctly. This is new behavior with Mavericks, so it is likely that Apple in their wonderful competence changed something. Does a work around exist yet ?

 

Both of these are not show stoppers, but they do get annoying after awhile and probably should be looked at by whomever is doing Cadsoft's Mac support

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest +1
    James Morrison wrote on Sat, 19 April 2014 21:54 Jorge Garcia wrote on Mon, 17 February 2014 11:52 Hi Everyone, If anyone can reproduce or has run into the issues Matt is seeing please reply. I need to…
Parents
  • makenoise
    0 makenoise over 11 years ago

    I have all of the issues op mentions.

     

    I waited until I absolutely had to install Mavericks, which was just a couple weeks ago.

     

    I find Eagle is almost un-usable. All of my keyboard shortcuts that use the Option key no longer work either.

     

    I'm still running 6.5

     

    I wish Cadsoft would fix this stuff. I'm seriously considering making the move to a new software package if they do not.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • makenoise
    0 makenoise over 11 years ago

    I have all of the issues op mentions.

     

    I waited until I absolutely had to install Mavericks, which was just a couple weeks ago.

     

    I find Eagle is almost un-usable. All of my keyboard shortcuts that use the Option key no longer work either.

     

    I'm still running 6.5

     

    I wish Cadsoft would fix this stuff. I'm seriously considering making the move to a new software package if they do not.