EAGLE User Support (English) polygon void ver 4.16r2
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
  • Replies 1 reply
  • Subscribers 177 subscribers
  • Views 165 views
  • Users 0 members are here
Related

polygon void ver 4.16r2

autodeskguest
autodeskguest over 17 years ago

Sorry if this is an old subject, only just got round to using my v4.16

 

Is there a way to do a polgon void on a "normal" layer used for drawing

polygons to be used for power supplies . I want a permanent void in a

polygon(1). So far I can only think to draw another polygon(2) with a higher

rank inside (1) and then delete this polygon(2) to leave the void.  However

this is prone to forgetting to do to the delete.

 

TIA for any advice,

 

Dave Wells

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    David Wells wrote:

    Sorry if this is an old subject, only just got round to using my v4.16

     

    Is there a way to do a polgon void on a "normal" layer used for

    drawing polygons to be used for power supplies . I want a permanent

    void in a polygon(1). So far I can only think to draw another

    polygon(2) with a higher rank inside (1) and then delete this

    polygon(2) to leave the void.  However this is prone to forgetting to

    do to the delete.

     

    This has come up a few times.  You can use two overlapping U-shaped polygons

    (same rank), each drawn around the void area.

     

    Merry Christmas,

     

    Bert Menkveld

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    David Wells wrote:

    Sorry if this is an old subject, only just got round to using my v4.16

     

    Is there a way to do a polgon void on a "normal" layer used for

    drawing polygons to be used for power supplies . I want a permanent

    void in a polygon(1). So far I can only think to draw another

    polygon(2) with a higher rank inside (1) and then delete this

    polygon(2) to leave the void.  However this is prone to forgetting to

    do to the delete.

     

    This has come up a few times.  You can use two overlapping U-shaped polygons

    (same rank), each drawn around the void area.

     

    Merry Christmas,

     

    Bert Menkveld