EAGLE User Support (English) Make PCB etched route wider?
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
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 180 subscribers
  • Views 1990 views
  • Users 0 members are here
Related

Make PCB etched route wider?

velocity
velocity over 11 years ago

Hello everyone,  I'm new to Eagle Cad and was wondering if anyone could give me a tip on widening the etched route lines when I go to make a PCB layout.  I'm not referring to the actual traces but the lines that my CNC machine would etch out the copper during milling.  Problem is that the smallest endmill I have is a 1mm and when I go to process the G-Code, it fails because the etch lines are smaller than my endmill.  Any help would be very much appreciated!  Thanks!

 

image

  • Sign in to reply
  • Cancel
Parents
  • velocity
    0 velocity over 11 years ago

    Hi guys,

     

    Thanks for the replies.  I went through and tried what you advised but all it does is thicken the trace and not the etched lines (the lines that show up black) -- which would be the lines that are milled by the CNC endmill (see image).

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • GRPZijlstra
    0 GRPZijlstra over 11 years ago in reply to velocity

    That is weird. I made a few screenshots.

    image

    I made this simple board with some normal .016 inch traces. The dotted line is the plygon for the copper-pour (ground pour).

     

    I then hit the ratsnest icon to get the plygon filled using standard .016 inch isolation :

    image

    I then selected the polygon (either right-click -> properties or using the 'i' icon) and changed the isolate to 0.032 :

    image

    As you can see this should do what you need (unless the blue plane in your board is not done using a polygon with copper-pour, but it looks like it is).

     

    Of course, the distance between normal traces (not between a trace and a copper-pour/plane) is controlled by you if you route manually, or by the clearance parameter in the DRC settings when using the autorouter as Mogens indicated.

     

    Hope this helps,

    Guido

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • velocity
    0 velocity over 11 years ago in reply to GRPZijlstra

    Thank you, Guido! (and everyone else as well) That was the ticket!  My issue was that I was right-clicking the properties for the trace and not for the polygon.  Once you showed me your screenshots, I figured it out and it works great now!

     

    Thanks so much!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • velocity
    0 velocity over 11 years ago in reply to GRPZijlstra

    Thank you, Guido! (and everyone else as well) That was the ticket!  My issue was that I was right-clicking the properties for the trace and not for the polygon.  Once you showed me your screenshots, I figured it out and it works great now!

     

    Thanks so much!