Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) via restring and clearance to the ground plane
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 187 subscribers
  • Views 495 views
  • Users 0 members are here
Related

via restring and clearance to the ground plane

autodeskguest
autodeskguest over 17 years ago

Hello.

 

After I read several postings about multilayer board, via, clearance,

etc from this newsgroup, I have got some questions about via restring

and clearance to the ground plane.

 

I want to create 6 layer board with Eagle as the following layer

configuration.

 

1 - signal

2 - ground

3 - signal

4 - vcc ( 3.3V, 2.5V, 1.2V )

5 - ground

15 - signal

 

According to Martin's Q&A, "6 layer board and 2 GND supply planes"

at 2007/11/08, defining two ground plane as supply layer is not allowed.

So I have to create ground layer(2 & 5) with a polygon.

 

In addition, as layer 4 has multiple nets, I have to create vcc layer(4)

with polygons.

 

Now, if a via is connected from the layer 15(signal) to layer 3(signal),

according to Tomas Pribyl's Q&A, "Via on 4-layers PCB" at 2006/06/02,

"pad of via and isolation gap are generated even if via is not connected to

GND or VCC". Therefore, it will create the large gap in layer 5(ground)

and layer 4(vcc) in my case. Sadly, annulus isolate or gap settings

at supply tab in the DRC settings has no effect on polygon-created

supply layer. (It works only on the supply layer.)

 

The answer to the question was to set the via inner layer

restring to zero in the DRC settings. It will work fine for ground and vcc

layer. But, the problem is in layer 3(signal). layer 3 can't have

the restring at all because via inner layer restring is set to zero.

 

The question,

1) Is there any ways to make annulus isolate DRC setting work on

polygon-created supply layer?

2) is there any ways to make two different inner layer have two different

via

restring?

 

Thanks in advance.

 

Best regards.

--

Taeho Oh ( ohhara@postech.edu , ohhara@plus.or.kr )

http://ohhara.sarang.net

Postech ( Pohang University of Science and Technology )

http://www.postech.edu

Digital Media Professionals Inc.

http://www.dmprof.com

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 17 years ago

    Taeho Oh schrieb:

    Hello.

     

    After I read several postings about multilayer board, via, clearance,

    etc from this newsgroup, I have got some questions about via restring

    and clearance to the ground plane.

     

    I want to create 6 layer board with Eagle as the following layer

    configuration.

     

    1 - signal

    2 - ground

    3 - signal

    4 - vcc ( 3.3V, 2.5V, 1.2V )

    5 - ground

    15 - signal

     

    According to Martin's Q&A, "6 layer board and 2 GND supply planes"

    at 2007/11/08, defining two ground plane as supply layer is not allowed.

    So I have to create ground layer(2 & 5) with a polygon.

     

    In addition, as layer 4 has multiple nets, I have to create vcc layer(4)

    with polygons.

     

    Now, if a via is connected from the layer 15(signal) to layer 3(signal),

    according to Tomas Pribyl's Q&A, "Via on 4-layers PCB" at 2006/06/02,

    "pad of via and isolation gap are generated even if via is not connected to

    GND or VCC". Therefore, it will create the large gap in layer 5(ground)

    and layer 4(vcc) in my case. Sadly, annulus isolate or gap settings

    at supply tab in the DRC settings has no effect on polygon-created

    supply layer. (It works only on the supply layer.)

     

    The answer to the question was to set the via inner layer

    restring to zero in the DRC settings. It will work fine for ground and vcc

    layer. But, the problem is in layer 3(signal). layer 3 can't have

    the restring at all because via inner layer restring is set to zero.

     

    The question,

    1) Is there any ways to make annulus isolate DRC setting work on

    polygon-created supply layer?

    2) is there any ways to make two different inner layer have two different

    via

    restring?

     

    Sorry, this is not possible. There is one restring setting which is

    valid for all inner layers.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 17 years ago

    Taeho Oh schrieb:

    Hello.

     

    After I read several postings about multilayer board, via, clearance,

    etc from this newsgroup, I have got some questions about via restring

    and clearance to the ground plane.

     

    I want to create 6 layer board with Eagle as the following layer

    configuration.

     

    1 - signal

    2 - ground

    3 - signal

    4 - vcc ( 3.3V, 2.5V, 1.2V )

    5 - ground

    15 - signal

     

    According to Martin's Q&A, "6 layer board and 2 GND supply planes"

    at 2007/11/08, defining two ground plane as supply layer is not allowed.

    So I have to create ground layer(2 & 5) with a polygon.

     

    In addition, as layer 4 has multiple nets, I have to create vcc layer(4)

    with polygons.

     

    Now, if a via is connected from the layer 15(signal) to layer 3(signal),

    according to Tomas Pribyl's Q&A, "Via on 4-layers PCB" at 2006/06/02,

    "pad of via and isolation gap are generated even if via is not connected to

    GND or VCC". Therefore, it will create the large gap in layer 5(ground)

    and layer 4(vcc) in my case. Sadly, annulus isolate or gap settings

    at supply tab in the DRC settings has no effect on polygon-created

    supply layer. (It works only on the supply layer.)

     

    The answer to the question was to set the via inner layer

    restring to zero in the DRC settings. It will work fine for ground and vcc

    layer. But, the problem is in layer 3(signal). layer 3 can't have

    the restring at all because via inner layer restring is set to zero.

     

    The question,

    1) Is there any ways to make annulus isolate DRC setting work on

    polygon-created supply layer?

    2) is there any ways to make two different inner layer have two different

    via

    restring?

     

    Sorry, this is not possible. There is one restring setting which is

    valid for all inner layers.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

    CadSoft Support -- hotline@cadsoft.de

    FAQ: http://www.cadsoft.de/faq.htm