EAGLE User Support (English) Package Pad Sizes Revert to "Auto" after a Custom size is selected
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
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 287 views
  • Users 0 members are here
Related

Package Pad Sizes Revert to "Auto" after a Custom size is selected

Former Member
Former Member over 11 years ago

Hi, I am trying to create a custom thru-hole component that must have a pad with a smaller diameter than the size generated with the "auto" selection. I can set the pad size when I create the component, but when the part is inserted into the PCB the pad sizes have reverted to the "auto" selection with much larger diameter. I can then go back and open the component and it has the correct size pads. As seen in the attached screen shot, the component on the left is placed on the circuit board. When I right-click the component and open the package, you can see the pads are much smaller and not touching as in the PCB version. Any suggestions?

Fullscreen contentimage_30020.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 26/02/14 21:24, Rick Vaughn wrote:

    Hi, I am trying to create a custom thru-hole component that must have a

    pad with a smaller diameter than the size generated with the "auto"

    selection. I can set the pad size when I create the component, but when

    the part is inserted into the PCB the pad sizes have reverted to the

    "auto" selection with much larger diameter. I can then go back and open

    the component and it has the correct size pads. As seen in the attached

    screen shot, the component on the left is placed on the circuit board.

    When I right-click the component and open the package, you can see the

    pads are much smaller and not touching as in the PCB version. Any

    suggestions?

     

    Check your DRC settings, particularly "restring"

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    Thanks for the help! Apparently, the restring overrides the custom setting (even though the pad thickness was greater than the minimum setting in the restring parameter. I had to change the % from 25 to 18 to allow the custom pads sizes to exist on the component when placed on the circuit board. This is a new one on me!  I will verify I have not caused any "new" problems when I lowered the restring % to 18.

    I attached a short description of the problem I encountered with the solution. This may help someone else if they come across the same problem with custom pad sizes (that are less than the default Restring size calculation).

    Thanks again! Rick

    Attachments:
    imageRestringNotes.pdf
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    Thanks for the help! Apparently, the restring overrides the custom setting (even though the pad thickness was greater than the minimum setting in the restring parameter. I had to change the % from 25 to 18 to allow the custom pads sizes to exist on the component when placed on the circuit board. This is a new one on me!  I will verify I have not caused any "new" problems when I lowered the restring % to 18.

    I attached a short description of the problem I encountered with the solution. This may help someone else if they come across the same problem with custom pad sizes (that are less than the default Restring size calculation).

    Thanks again! Rick

    Attachments:
    imageRestringNotes.pdf