Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Adding despiking capacitors
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 17 replies
  • Subscribers 193 subscribers
  • Views 2971 views
  • Users 0 members are here
Related

Adding despiking capacitors

scheveningen
scheveningen over 12 years ago

Hi Jorge,

 

I have designed my schematic in Eagle and I want to add despiking capacitors. They have to be close to the chip.

The manual is saying something about the INVOKE command, but not very clear? How do I add these small

despiking capacitors?

 

 

Please advise,

Very respectfully,

peter

(from The Hague Holland)

  • Sign in to reply
  • Cancel
Parents
  • AnalogNotes
    0 AnalogNotes over 12 years ago

    You can add these capacitors in the schematic like you would add any other part and connect them to the chip the way you would connect any other parts.  On the schematic, it doesn't matter where you place the capacitors physically, but they should be connected directly to the chip electrically.  When you make your board, then you can place the parts very close together.

     

    The INVOKE command is used for the chips themselves and allows you to place part of the chip on your schematic.  For example, if you have a quad op amp, you can invoke any of the four op amp circuits.  If you don't use one or more of the op amps, you don't have to invoke them and they won't show on the schematic.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • AnalogNotes
    0 AnalogNotes over 12 years ago

    You can add these capacitors in the schematic like you would add any other part and connect them to the chip the way you would connect any other parts.  On the schematic, it doesn't matter where you place the capacitors physically, but they should be connected directly to the chip electrically.  When you make your board, then you can place the parts very close together.

     

    The INVOKE command is used for the chips themselves and allows you to place part of the chip on your schematic.  For example, if you have a quad op amp, you can invoke any of the four op amp circuits.  If you don't use one or more of the op amps, you don't have to invoke them and they won't show on the schematic.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • scheveningen
    0 scheveningen over 12 years ago in reply to AnalogNotes

    Dear Don Hersey,  mcb1 + Doug Wellington,

     

    Wow!!!! Very fast and awesome response!! Thank you so much gentlemen. Yes, very correct, one just has to place them in the schematic and then later move them closer to the chips. I am now after I read the insight on, "over use" of these caps........thinking of.......instead of one cap per chip, perhaps will use......one cap per two chips. It is very easy to overdo this decoupling/despiking thing. The currents will start to breath instead of flow on the tracks.

     

    I am designing my power tracks 3 times ticker then my signal tracks also, much better for the overall impedance.

     

    Thx again gentlemen!

    Cheers,

    peter