Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Etch Resist from InkJet Printer?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 186 subscribers
  • Views 1988 views
  • Users 0 members are here
Related

Etch Resist from InkJet Printer?

autodeskguest
autodeskguest over 17 years ago

I've got an InkJet Printer that will print on CDs and DVDs.  Is it possible

to print etch resist directly onto a PCB?

 

--

 

Nigel M

 

If I'm discussing apples, please don't suggest bananas

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Nigel Molesworth wrote:

    I've got an InkJet Printer that will print on CDs and DVDs.

     

    I got an idea...

     

    If i sticks to that plastic surface, i would guess it can stick to the

    photo-reesist too...?

     

    So if you work in a dark room and print on the photo resist, then expose

    etc as normal?

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    On Sat, 10 Jan 2009 12:00:30 -0800, "Ron" <viaEagleForum@RGMEusa.com>

    wrote:

     

    You can use a laser printer and then use a hot (clothes) iron to transfer

    the toner to the pcb. The toner is plastic and acts as a resist. See:

    http://another-electronics.blogspot.com/2008/09/how-to-make-pcbs-with-laser-printer.html

    You're not going to get fine pitch, though it should work ok if all parts

    are through-hole (~ 0.1" pitch) and you keep your traces fairly large.

     

    I use toner transfer whenever I want a quick prototype. I have no

    problems at all with SOIC (1.27mm) or 10 mil traces. Recently, I did

    an MLP-28 (0.5mm). That was a little problematic, but I got it working

    in the end, by using the printers "econo" mode to get a thinner layer

    of toner so it squished less out.

     

    I use a laminator for the ironing. Much more repeatable and

    predictable than a clothes iron.

     

    IMHO neither method is good for more than 1 layer though, because of the

    difficulty in registration (lining patterns up on both sides).

     

    I have not tried two layers with toner transfer yet (I try very hard

    to keep my designs to single layer), but with photo transfer, I got

    very good results. I used a frame made from scrap laminate, and then

    taped the two films onto the frame first, before sliding the board in

    between the films. A two-sided UV light box helps, because it takes

    some care to turn the fixture without moving the board inside the

    frame.

    --

    RoRo

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    On Sat, 10 Jan 2009 15:33:27 +0000, Nigel Molesworth

    <reply@thegroup.email.invalid> wrote:

     

    I've got an InkJet Printer that will print on CDs and DVDs.  Is it possible

    to print etch resist directly onto a PCB?

     

    I've never tried it, but I did a bit of research before I bought my

    previous printer. That's a while ago, so things may have changed.

     

    The biggest problem is that most inks are not water proof, so they

    will wash off in the etch bath. Some inks, I think HP's pigment based

    inks, can be used.

     

    The next problem is that the ink may not bind properly to the copper

    surface. Ink is intended to soak into the paper, but, again, some inks

    suitable for glossy photo paper may work.

     

    What it boils down to, is finding the right ink.

    --

    RoRo

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    "Nigel Molesworth" <reply@thegroup.email.invalid> wrote in message

    news:tqfhm4hj3e62t70v7q8li96pi8adv2oh3a@4ax.com...

    I've got an InkJet Printer that will print on CDs and DVDs.  Is it

    possible

    to print etch resist directly onto a PCB?

     

    --

     

    Nigel M

     

    If I'm discussing apples, please don't suggest bananas

     

    In general, no. Because (usually) standard inkjet printer ink will not

    protect against etching.

     

    You can use a laser printer and then use a hot (clothes) iron to transfer

    the toner to the pcb. The toner is plastic and acts as a resist. See:

    http://another-electronics.blogspot.com/2008/09/how-to-make-pcbs-with-laser-printer.html

    You're not going to get fine pitch, though it should work ok if all parts

    are through-hole (~ 0.1" pitch) and you keep your traces fairly large.

     

    If you need fine pitch then try the photo process. See:

    http://www.action-electronics.com/pcb.htm

    for some methods & supplies.

     

    IMHO neither method is good for more than 1 layer though, because of the

    difficulty in registration (lining patterns up on both sides). The photo

    method should allow up to 5mm pitch (with practice, temperature makes a

    difference in photo development time required), so this can be used with SMD

    parts.