EAGLE User Support (English) Is it possible to make a resistor pack symbol where the resistor values are independent?
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
  • State Suggested Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 181 subscribers
  • Views 639 views
  • Users 0 members are here
Related

Is it possible to make a resistor pack symbol where the resistor values are independent?

Former Member
Former Member over 11 years ago

I have a customer who prefer as many of the resistors in their designs be in 8 pin DIP resistor packs, so the resistors can be changed out easily. Is it possible to make a single device made up of four independent resistors? I could just write the resistor values onto the schematic, but I was hoping for a cleaner way.

 

Thanks in advance.

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    0 dukepro over 11 years ago

    On 04/24/2014 08:37 PM, Josh Pyne wrote:

    I have a customer who prefer as many of the resistors in their designs

    be in 8 pin DIP resistor packs, so the resistors can be changed out

    easily. Is it possible to make a single device made up of four

    independent resistors? I could just write the resistor values onto the

    schematic, but I was hoping for a cleaner way.

     

    Josh,

     

    There isn't a clean way of doing this.  I fiddled around with it a bit

    to no avail.  I even tried adding an attribute to each gate - no joy.

     

    Attached is a library file with a DIL08 package without the pads.  I

    added marks where the PTH pads from the resistor package should be

    centered.  This can be added to your board without affecting the

    schematic, and used as a guide in placing the individual resistors.  You

    may also need to create a 2-pad package for each resistor with 300mil

    spacing between the pads.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dukepro
    0 dukepro over 11 years ago

    On 04/24/2014 08:37 PM, Josh Pyne wrote:

    I have a customer who prefer as many of the resistors in their designs

    be in 8 pin DIP resistor packs, so the resistors can be changed out

    easily. Is it possible to make a single device made up of four

    independent resistors? I could just write the resistor values onto the

    schematic, but I was hoping for a cleaner way.

     

    Josh,

     

    There isn't a clean way of doing this.  I fiddled around with it a bit

    to no avail.  I even tried adding an attribute to each gate - no joy.

     

    Attached is a library file with a DIL08 package without the pads.  I

    added marks where the PTH pads from the resistor package should be

    centered.  This can be added to your board without affecting the

    schematic, and used as a guide in placing the individual resistors.  You

    may also need to create a 2-pad package for each resistor with 300mil

    spacing between the pads.

     

    HTH,

        - Chuck

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer