EAGLE User Support (English) LTspice Standard Libraries & Drill Sizes
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 177 subscribers
  • Views 269 views
  • Users 0 members are here
Related

LTspice Standard Libraries & Drill Sizes

Former Member
Former Member over 11 years ago


Hi my name is Chris Escalante and I am a EE.  I have been tasked with updating my company Eagle files from version 3.55 into 6.4.0 and to be able to import/export these files into LTSpice.  Eagle has converted the files but when I try to export I get errors.  I have added several industry parts to the LTSpice standard library set (i.e. standard.dio, standard.cap), which I don't believe have a .sub file.  Every example of getting LTSpice and Eagle to work together uses a .sub file to verify spiceorder and to connect the LTSpice model to the Eagle model.  I have added every LTSpice assembly file and every .sub to Eagle and I still get the ulp error "Different Quantity of SpiceOrder and PINs in symbol CAP of par C1.  Please Check Symbol."  I have added spice order to the part tried to link it to a standard file in LTSpice, although I am not sure if these files carry the .lib extension or the .sub extension; nevertheless nothing works.  The standard file for capacitors is where the LTSpice model is stored.  Why is there not a designated file in Eagle to save cmp files from LTSpice, which is where the standard libraries are saved in LTSpice, and/or can anyone give me any insight into what else I might try?  I am also having difficulty getting drill sizes to update in the silkscreen after I change the drill sizes in the part.  I am not sure I can attach the circuit file as it is proprietary.  Thanks in advance for any help!

 

UPDATE:

I just noticed a more fundimental problem with the conversion from 3.55 to 6.4.0 that I didn't notice before.  I am getting this error on most of the parts in the schematic "Package variant "  of deviceset 524396-002@5 does not exist in current library.  Please adjust the library paths or export the drawing libraries first!"  I have searched all company libraries for 524396-002@5 but it does not exist with the "@5" and I have tried to create one but it still gives me the same error.  I have also tried to change the package but it does not give me any other options but 524396-002@5 in the window.  The other parts give the same error except with a different part number and an "@5" at the end.  If I didn't mention before I have 2 years of experience with LTspice, but I just started working with Eagle.  What am I doing wrong or how can I get the libraries set correctly so I can make some progress updating the schematics?  Thanks in advance for an help!

Chris

 

Message was edited by: Chris Escalante

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    I just noticed a more fundimental problem with the conversion from 3.55

    to 6.4.0 that I didn't notice before.  I am getting this error on most

    of the parts in the schematic "Package variant "  of deviceset

    524396-002@5 does not exist in current library.  Please adjust the

    library paths or export the drawing libraries first!"  I have searched

    all company libraries for 524396-002@5 but it does not exist with the

    "@5" and I have tried to create one but it still gives me the same

    error.  I have also tried to change the package but it does not give me

    any other options but 524396-002@5 in the window.  The other parts give

    the same error except with a different part number and an "@5" at the

    end.  If I didn't mention before I have 2 years of experience with

    LTspice, but I just started working with Eagle.  What am I doing wrong

    or how can I get the libraries set correctly so I can make some progress

    updating the schematics?  Thanks in advance for an help!

    Chris

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/111116