EAGLE User Support (English) Pin swapping has no effect?
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
  • State Not Answered
  • Replies 4 replies
  • Subscribers 178 subscribers
  • Views 541 views
  • Users 0 members are here
  • eagle
  • pin
  • swap
  • swaplevel
  • symbol
Related

Pin swapping has no effect?

Former Member
Former Member over 11 years ago

I am using Eagle v. 6.5. I have designed a symbol for a device that allows me to swap some pins. However, pin swapping does not seem to work. In the schematic I clicked on the pin swap button, then clicked the two pins I want to swap. The pin numbers stays the same...

 

I tried this with a 7400-series NAND-gate as well. No effect here either. Is this a bug or am I doing something wrong? I am sure that the pins have the same swaplevel.

 

Thanks in advance :-)

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 11 years ago

    Am 08.05.2014 17:24, schrieb Peter Haagerup:

    I am using Eagle v. 6.5. I have designed a symbol for a device that

    allows me to swap some pins. However, pin swapping does not seem to

    work. In the schematic I clicked on the pin swap button, then clicked

    the two pins I want to swap. The pin numbers stays the same...

     

    I tried this with a 7400-series NAND-gate as well. No effect here

    either. Is this a bug or am I doing something wrong? I am sure that the

    pins have the same swaplevel.

     

    What number of swap level?

    0 is never swap!

     

    You can only swap pin with same level

    1 <-> 1

    2 <-> 2

    3 <-> 3

    ...

     

    Check the swap level of the pin on the symbol

    CHANGE Swaplevel  ...

     

     

    ***

    Um das Original zu lesen, und auch zuverlässig angehängte Dateien

    bereitstellen zu können, benutzen Sie news.cadsoft.de und einen

    funktionierenden News-Reader wie Thunderbird!

    ***

     

    Mit freundlichen Grüßen / Best regards

     

    Alfred Zaffran

    --

    ______________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Thomas Liratsch

    ______________________________________________________________

    EAGLE V6.5 availabe now!

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Thanks for your reply. Yes, I am aware of the swap levels. I have double checked and it still does not work. It is supposed to swap the pin numbers of the two swapped pins, right? Nothing happens - the symbol stays the same. Could this be a bug? I am using the Mac OS X version of Eagle 6.5, standard edition with schematic and board editor (no auto router) - I have not tried this on Windows or Linux. Maybe someone could try this in Eagle v. 6.5 and report if it works or not.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 11 years ago in reply to Former Member

    Thanks for your reply. Yes, I am aware of the swap levels. I have double checked and it still does not work. It is supposed to swap the pin numbers of the two swapped pins, right? Nothing happens - the symbol stays the same. Could this be a bug? I am using the Mac OS X version of Eagle 6.5, standard edition with schematic and board editor (no auto router) - I have not tried this on Windows or Linux. Maybe someone could try this in Eagle v. 6.5 and report if it works or not.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    Peter Haagerup wrote on Fri, 09 May 2014 07:50

    Thanks for your reply. Yes, I am aware of the swap levels. I have

    double

    checked and it still does not work. It is supposed to swap the pin

    numbers of the two swapped pins, right? Nothing happens - the symbol

    stays the same. Could this be a bug? I am using the Mac OS X version

    of

    Eagle 6.5, standard edition with schematic and board editor (no auto

    router) - I have not tried this on Windows or Linux. Maybe someone

    could

    try this in Eagle v. 6.5 and report if it works or not.

     

     

    Do you have the pin layer on in the schematic?  I believe the pin layer

    must be on in order to actually select the pins.

     

    James.

    --

    James Morrison  ~~~  Stratford Digital

     

    Specializing in CadSoft EAGLE

    • Online Sales to North America

    • Electronic Design Services

     

    Take advantage of v7 License Promotion right now at

    http://www.eaglecentral.ca

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to Former Member

    "Peter Haagerup"  skrev i nyhetsmeldingen:

    377880087.11399636283539.JavaMail.jive@flmspu-csapp-02.premierfarnell.com

    ...

    Thanks for your reply. Yes, I am aware of the swap levels. I have double

    checked and it still does not work. It is supposed to swap the pin

    numbers of the two swapped pins, right? Nothing happens - the symbol

    stays the same. Could this be a bug? I am using the Mac OS X version of

    Eagle 6.5, standard edition with schematic and board editor (no auto

    router) - I have not tried this on Windows or Linux. Maybe someone could

    try this in Eagle v. 6.5 and report if it works or not.

     

    Im sure this works. The symbol will not change, but the nets will swap (on

    schematic).

    Make sure you dont mix pin swaplevel this with gate swaplevel.

     

    Enable all layers in library symbol editor (even if it gets a bit messy) and

    show us a screengrab of it and it will be sorted in notime image

     

    Regards,