EAGLE User Support (English) multiple V+ pins custom part
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
  • State Not Answered
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 273 views
  • Users 0 members are here
  • multiple
  • pins
  • part
  • custom
Related

multiple V+ pins custom part

Former Member
Former Member over 11 years ago

I'm trying to create a custom part for a LT1210 amplifier.

 

The problem I have is that different packages have different number of V+ pins. Do I need to create a separate schematic for each package dependent on the number of V+ pins or is there a way to have a single V+ pin in the schematic and then join the V+ pins together in the part dependent upon the footprint?

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Am 21.05.2014 02:40, schrieb Ross Williamson:

    I'm trying to create a custom part for a LT1210 amplifier.

     

    The problem I have is that different packages have different number of

    V+ pins. Do I need to create a separate schematic for each package

    dependent on the number of V+ pins or is there a way to have a single V+

    pin in the schematic and then join the V+ pins together in the part

    dependent upon the footprint?

     

    Please use option Append in CONNECT menu, to connect more at one

    PAD/SMD on a PIN.

     

    Please read also HELP CONNECT

     

     

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/113416

     

     

     

    ***

    Um das Original zu lesen, und auch zuverlässig angehängte Dateien

    bereitstellen zu können, benutzen Sie news.cadsoft.de und einen

    funktionierenden News-Reader wie Thunderbird!

    ***

     

    Mit freundlichen Grüßen / Best regards

     

    Alfred Zaffran

    --

    ______________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Thomas Liratsch

    ______________________________________________________________

    EAGLE V6.5 availabe now!