EAGLE User Support (English) Installation of update
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
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 179 subscribers
  • Views 349 views
  • Users 0 members are here
Related

Installation of update

Former Member
Former Member over 11 years ago

I have only used Eagle for one day, so this question is as newbie as it can be:

Can I install a new version of Eagle (in this case, update from 6.5.0 to 6.6.0) over the existing version (in the same folder)? Or do I have to install it in a new folder and then uninstall the previous version?

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 6/3/2014 7:22 AM, Olav S. Flaa wrote:

    I have only used Eagle for one day, so this question is as newbie as it

    can be:

    Can I install a new version of Eagle (in this case, update from 6.5.0 to

    6.6.0) over the existing version (in the same folder)? Or do I have to

    install it in a new folder and then uninstall the previous version?

     

    Hi Olav,

     

    By default, every installation of EAGLE stands alone and is unaware of

    previous installs on the machine. I would advise against installing

    EAGLE in the same location of your previous install since you risk

    overwriting any libraries files you may have stored in the lbr folder.

     

    hth,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    Ok, thanks a lot for your help!