EAGLE User Support (English) Will ever be Eagle using real time GPU rendering?
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 181 subscribers
  • Views 546 views
  • Users 0 members are here
Related

Will ever be Eagle using real time GPU rendering?

Former Member
Former Member over 11 years ago

Hello,

 

I would like to ask if eagle will ever be using GPU rendering instead of CPU, which it using now. It's quite uncomfortable to get lags (I have core i5 3570K CPU) when Im routeng 4/6 layer PCB with polygons etc. Also making polygons more transparent than traces will be great, like Altium Designer doing it. I would love to buy version 7 of eagle, if it can do this.

 

Thank you very much.

 

Best Regards,

Jaroslav Dohnal

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 06/06/14 00:28, Jaroslav Dohnal wrote:

    Hello,

     

    I would like to ask if eagle will ever be using GPU rendering instead of

    CPU,

     

    I'm pretty sure it does! Certainly when my (ancient) Athlon box reverted

    to non-accelerated Qt it had a big impact on Eagle's performance.

     

    The thing is, Eagle uses a third-party graphics library (Qt) which will

    use GPU rendering if the base system is configured right. I'm not sure

    how this works out on Windows or Mac, but certainly on Linux it is quite

    possible to get Qt working that way.

     

    Cheers,

    Rob

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • AnalogNotes
    0 AnalogNotes over 11 years ago

    Which operating system are you using?  I'm using a five year old Core2 Quad Q8200 with 8GB of RAM and Windows Vista 64 bit with no lags...

     

    FWIW, I always use "rip @" to clear polygons (turn them into outlines) while I'm routing...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago

    Hello, I'm using Windows 8.1 64bit, i5 3570K, 8GB RAM, GTX 760 2GB VRAM. I'm not sure if it using any GPU lib on Windows, because when I scroll in or out, it uses GPU at about 2, 3%...also I have detection program which shows me which program using GPU and eagle didn't doing it. Altium Designer 14 definitely using GPU rendering over DirectX 10.

     

    These lags isn't lags as you may think...it just renders at about 2 - 5 FPS.