EAGLE User Support (English) Will ever be Eagle using real time GPU rendering?
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
  • State Not Answered
  • Replies 3 replies
  • Subscribers 181 subscribers
  • Views 546 views
  • Users 0 members are here
Related

Will ever be Eagle using real time GPU rendering?

Former Member
Former Member over 11 years ago

Hello,

 

I would like to ask if eagle will ever be using GPU rendering instead of CPU, which it using now. It's quite uncomfortable to get lags (I have core i5 3570K CPU) when Im routeng 4/6 layer PCB with polygons etc. Also making polygons more transparent than traces will be great, like Altium Designer doing it. I would love to buy version 7 of eagle, if it can do this.

 

Thank you very much.

 

Best Regards,

Jaroslav Dohnal

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 06/06/14 00:28, Jaroslav Dohnal wrote:

    Hello,

     

    I would like to ask if eagle will ever be using GPU rendering instead of

    CPU,

     

    I'm pretty sure it does! Certainly when my (ancient) Athlon box reverted

    to non-accelerated Qt it had a big impact on Eagle's performance.

     

    The thing is, Eagle uses a third-party graphics library (Qt) which will

    use GPU rendering if the base system is configured right. I'm not sure

    how this works out on Windows or Mac, but certainly on Linux it is quite

    possible to get Qt working that way.

     

    Cheers,

    Rob

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 06/06/14 00:28, Jaroslav Dohnal wrote:

    Hello,

     

    I would like to ask if eagle will ever be using GPU rendering instead of

    CPU,

     

    I'm pretty sure it does! Certainly when my (ancient) Athlon box reverted

    to non-accelerated Qt it had a big impact on Eagle's performance.

     

    The thing is, Eagle uses a third-party graphics library (Qt) which will

    use GPU rendering if the base system is configured right. I'm not sure

    how this works out on Windows or Mac, but certainly on Linux it is quite

    possible to get Qt working that way.

     

    Cheers,

    Rob