EAGLE User Support (English) Two questions; auto router and vias
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
  • State Verified Answer
  • Replies 9 replies
  • Answers 2 answers
  • Subscribers 179 subscribers
  • Views 744 views
  • Users 0 members are here
Related

Two questions; auto router and vias

Former Member
Former Member over 11 years ago

I have two questions:

 

1. Some components like terminal blocks and large electrolyte capacitors are supposed to be placed directly on the PCB which means that the pins must be soldered on the bottom layer. When I use the auto router feature, it makes traces both in the top and the bottom layer. Is there a way to tell the auto router feature that all connections to specific components have to be routed in the bottom layer? (What I did as a work around: Draw a rectangle/circle in the packages top-layer to define the size of the component, ran the auto router feature and then removed the temporary rectangles/circles.)

 

2. When I make VIAs on the board, the DRC gives a clearance error because the top and bottom traces overlap in the VIA-point. This happens even if the VIA is identical to those made by the auto router feature (which don't cause clearance error). What am I doing wrong?

 

Thanks for any help!

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    Am 09.06.2014 18:35, schrieb Olav S. Flaa:

    I have two questions:

     

    1. Some components like terminal blocks and large electrolyte capacitors

    are supposed to be placed directly on the PCB which means that the pins

    must be soldered on the bottom layer. When I use the auto router

    feature, it makes traces both in the top and the bottom layer. Is there

    a way to tell the auto router feature that all connections to specific

    components have to be routed in the bottom layer? (What I did as a work

    around: Draw a rectangle/circle in the packages top-layer to define the

    size of the component, ran the auto router feature and then removed the

    temporary rectangles/circles.)

     

    2. When I make VIAs on the board, the DRC gives a clearance error

    because the top and bottom traces overlap in the VIA-point. This happens

    even if the VIA is identical to those made by the auto router feature

    (which don't cause clearance error). What am I doing wrong?

     

    Thanks for any help!

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/115764

     

     

    1. Autorouter/General-Tab setting N/A into a layer will block the use.

    2. Can't say directly but something does not fit the design rules.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    Am 09.06.2014 18:35, schrieb Olav S. Flaa:

    I have two questions:

     

    1. Some components like terminal blocks and large electrolyte capacitors

    are supposed to be placed directly on the PCB which means that the pins

    must be soldered on the bottom layer. When I use the auto router

    feature, it makes traces both in the top and the bottom layer. Is there

    a way to tell the auto router feature that all connections to specific

    components have to be routed in the bottom layer? (What I did as a work

    around: Draw a rectangle/circle in the packages top-layer to define the

    size of the component, ran the auto router feature and then removed the

    temporary rectangles/circles.)

     

    2. When I make VIAs on the board, the DRC gives a clearance error

    because the top and bottom traces overlap in the VIA-point. This happens

    even if the VIA is identical to those made by the auto router feature

    (which don't cause clearance error). What am I doing wrong?

     

    Thanks for any help!

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/115764

     

     

    1. Autorouter/General-Tab setting N/A into a layer will block the use.

    2. Can't say directly but something does not fit the design rules.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 11 years ago in reply to autodeskguest

    Thanks for your reply!

     

    Unfortunately I can't block the top layer, I need to auto route using both the bottom and top layer. But the routing to/from a few specific components has to be on the bottom layer.