EAGLE User Support (English) Can't connect SMD pads
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
  • State Not Answered
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 1157 views
  • Users 0 members are here
Related

Can't connect SMD pads

Former Member
Former Member over 11 years ago

I designed my schematic using all SMD parts, but when I switched over to the board, I can't connect the air wires when manually routing. When I run the auto route, it connects the pads without a problem, but I much more prefer to run manual routing. If I add in through hole components, it connects the pads without an issue as well. I've made sure the trace starts over the pad, and connects over the other pad, but the air wire doesn't go away (even after cleaning up the rats nest) . When I highlight the net, it highlights the pads but not the trace, even though both the pads and trace are on the same layer. Any suggestions?

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On Sat, 05 Jul 2014 23:35:56 GMT, Alex Wende

    <noreply-261136@element14.com> wrote:

     

    I designed my schematic using all SMD parts, but when I switched over to

    the board, I can't connect the air wires when manually routing. When I

    run the auto route, it connects the pads without a problem, but I much

    more prefer to run manual routing. If I add in through hole components,

    it connects the pads without an issue as well. I've made sure the trace

    starts over the pad, and connects over the other pad, but the air wire

    doesn't go away (even after cleaning up the rats nest) . When I

    highlight the net, it highlights the pads but not the trace, even though

    both the pads and trace are on the same layer. Any suggestions?

     

    When you select the routing tool and click near the center of an SMD

    pad with an air wire going to it, what happens?  Normally the selected

    air wire is highlighted.  If the cursor turns into a four-pointed

    arrow (up, down, right, left) that means Eagle is not sure which

    starting point you mean because you are close to more than one

    starting point.  In that case you might have to right-click until the

    desired air wire and pad is highlighted.  Then you can left-click and

    begin routing.

     

    Robert Scott

    Hopkins, MN

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    On Sat, 05 Jul 2014 23:35:56 GMT, Alex Wende

    <noreply-261136@element14.com> wrote:

     

    I designed my schematic using all SMD parts, but when I switched over to

    the board, I can't connect the air wires when manually routing. When I

    run the auto route, it connects the pads without a problem, but I much

    more prefer to run manual routing. If I add in through hole components,

    it connects the pads without an issue as well. I've made sure the trace

    starts over the pad, and connects over the other pad, but the air wire

    doesn't go away (even after cleaning up the rats nest) . When I

    highlight the net, it highlights the pads but not the trace, even though

    both the pads and trace are on the same layer. Any suggestions?

     

    When you select the routing tool and click near the center of an SMD

    pad with an air wire going to it, what happens?  Normally the selected

    air wire is highlighted.  If the cursor turns into a four-pointed

    arrow (up, down, right, left) that means Eagle is not sure which

    starting point you mean because you are close to more than one

    starting point.  In that case you might have to right-click until the

    desired air wire and pad is highlighted.  Then you can left-click and

    begin routing.

     

    Robert Scott

    Hopkins, MN