EAGLE User Support (English) Can't connect SMD pads
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
  • State Not Answered
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 1158 views
  • Users 0 members are here
Related

Can't connect SMD pads

Former Member
Former Member over 11 years ago

I designed my schematic using all SMD parts, but when I switched over to the board, I can't connect the air wires when manually routing. When I run the auto route, it connects the pads without a problem, but I much more prefer to run manual routing. If I add in through hole components, it connects the pads without an issue as well. I've made sure the trace starts over the pad, and connects over the other pad, but the air wire doesn't go away (even after cleaning up the rats nest) . When I highlight the net, it highlights the pads but not the trace, even though both the pads and trace are on the same layer. Any suggestions?

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 07/05/2014 07:35 PM, Alex Wende wrote:

    I designed my schematic using all SMD parts, but when I switched over to

    the board, I can't connect the air wires when manually routing. When I

    run the auto route, it connects the pads without a problem, but I much

    more prefer to run manual routing. If I add in through hole components,

    it connects the pads without an issue as well. I've made sure the trace

    starts over the pad, and connects over the other pad, but the air wire

    doesn't go away (even after cleaning up the rats nest) . When I

    highlight the net, it highlights the pads but not the trace, even though

    both the pads and trace are on the same layer. Any suggestions?

     

    Make sure you're using the "route" command rather than the "wire"

    command, either through the action toolbar or command interface.

     

    -Reece

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 07/05/2014 07:35 PM, Alex Wende wrote:

    I designed my schematic using all SMD parts, but when I switched over to

    the board, I can't connect the air wires when manually routing. When I

    run the auto route, it connects the pads without a problem, but I much

    more prefer to run manual routing. If I add in through hole components,

    it connects the pads without an issue as well. I've made sure the trace

    starts over the pad, and connects over the other pad, but the air wire

    doesn't go away (even after cleaning up the rats nest) . When I

    highlight the net, it highlights the pads but not the trace, even though

    both the pads and trace are on the same layer. Any suggestions?

     

    Make sure you're using the "route" command rather than the "wire"

    command, either through the action toolbar or command interface.

     

    -Reece